MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! LSM9DS1 magnetometer interrupts - open-drain or push/pull?

Posted on May 08, 2017 at 01:17The LSM9DS1 data sheet shows that the accelerometer/gyroscope module's two interrupts can be configured either as open-drain or push/pull.  However, I am missing the description of the magnetometer module's interrupt. ...

LIS2DH full scale @ +/-16g stationory

Posted on May 15, 2017 at 15:36Hi,I am working on a project that is using LIS2DH sensor for measuring the acceleration along the X,Y and Z-axis. I have configured the IC as per the following configurations:-1>Using the 8-bit resolution to capture th...

LIS3DH Stream FIFO

Posted on May 16, 2017 at 01:47I configured the LIS3DH in stream FIFO mode. Then I set the WATERMARK level as 8 bytes and I poll the FIFO_SRC_REG to see if the WTM bit is 1 and then I collect the 8 bytes of data accumulated in FIFO. Now my problem i...

LIS3DH single and double click configure at the same time

Posted on May 19, 2017 at 10:50Hey guys, it is possible to configure single and double click at the same time? When I enable double and single click at the same time, it seems that the accelerometer only detect double click. Any solution to this ?#a...

HTS221 Humidity problem

Posted on May 12, 2017 at 12:04Hello. I have a problem with humidity measurement. Despite the proper value of temperature, te humidity is always over 100%. I'm using the official ST software. I'm wondering if it is a hardware problem ?The initializa...

Unico Lite GUI

Posted on May 16, 2017 at 18:23Hi, is there any pdf available relating to the operation of the Unico Lite GUI. I have version 2.0.0.0 installed but I cannot seem to get it to communicate with the LSM6DS3.Thanks#lsm6ds3 #unico-lite

daithi62 by Associate II
  • 1749 Views
  • 3 replies
  • 0 kudos

Resolved! LIS3MDL data interpretation

Posted on May 15, 2017 at 18:45Hello,I have the a question about LIS3MDL.I have read http://www.st.com/resource/en/datasheet/lis3mdl.pdf and an http://www.st.com/resource/en/application_note/dm00136626.pdf, but have no idea, how to interpret the dat...

LSM6DS3 linker error L6218E - LSM6DS3_IO_Read

Posted on May 09, 2017 at 11:39I am getting a linker error L6218E when compiling code for the LSM6DS3 Gyroscope. The error points to the LSM6DS3_IO_Read and LSM6DS3_IO_Write functions. These have been declared and are to be imported but there is no ...

daithi62 by Associate II
  • 1717 Views
  • 3 replies
  • 0 kudos

LIS3DH Click Interrupt

Posted on May 15, 2017 at 10:32Hey guys, I dunno what I add but seems I can't generate interrupt after I click on LIS3DH, here what I do.void Acc__EnableClickDetect(void){  LIS3DH_SetAxis(LIS3DH_X_ENABLE  |LIS3DH_Y_ENABLE | LIS3DH_Z_ENABLE );  LIS3D...