MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LIS2DHTR Reflow Issue

Posted on March 30, 2017 at 21:02Hello,     We are working with the LIS2DHTR and have had significant yield issues after running the board through the reflow oven.  For the next run we plan to lower the temperature.  But for now we are replacing the...

LSM6DSL Min/Max specifications for ODR (Output Data Rate)

Posted on March 21, 2017 at 15:35I'm using the LSD6DSL in an application where the sampling rate (ODR for the MEMs) is important. The ODR in the datasheet is only given as 'Typical'. Could I get a more precise specification for the ODR, e.g. min/max...

cn2 by Associate II
  • 627 Views
  • 1 replies
  • 0 kudos

use X-NUCLEO-53L0A1 satellites as proximity sensor

Posted on March 29, 2017 at 08:37Hi, I'm new with stm32 and mbed environment. I'm trying to use VL53L0X satellites as proximity/distance sensor but I have few unsolved questions: 1) in this datasheet I can see that only first six pin of satellites a...

www.st.com

Posted on April 03, 2017 at 12:56Apple watch accelerometer axis range Hi good morning,I'm developing an apple watch health care application. After a search i discover an ST microelectronics accelerometer sensor mounted on a system on a chip internal...

LIS3DH Interrupt INT1 Mode Not Firing

Posted on April 07, 2017 at 08:14I'm using the LIS3DH set at 1 Hz ODR.  My SPI hardware seems to be working since DATA_RDY interrupts come in fine at a steady 1 second interval and the accelerometer data looks good.  In fact I get good data at all s...

Programming (setup) of LSM6DSL IMU via 4-wire SPI

Posted on April 06, 2017 at 21:58Couple of questions regarding the LSM6DSL (iNEMO intertial module) setup via the SPI interface.1. Should it possible to program the IMU at 10 MHz SPI interface or does the programming need to be done a slower speed?2...

gaurav2 by Associate II
  • 592 Views
  • 0 replies
  • 0 kudos

Resolved! LSM9DS1 input-high voltage for CS inputs?

Posted on April 05, 2017 at 00:02Although powering an LSM9DS1 with 2.8V to VDDIO and VDD, I would like to use a 1.8V-logic line for one of the chip selects for ease of retrofitting an existing design with minimum upheaval.  The line is push-pull, no...

VL53L0X X-NUCLEO-53L0A1 Cover Glass

Posted on September 02, 2016 at 18:04We are developing a product using the VL53L0X IR Time-Of-Flight sensor. The sensor must be inside a plastic case looking through a IR transmissible window material. To test such an arrangement the X-NUCLEO-53L0A1...

FIT rate Value for IC LIS3DHTR ?

Posted on April 06, 2017 at 08:15for Doing FMEDA I need FIT rate value for IC LIS3DHTRIn data sheet ,reliability data  it is not mentioned.