MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

FIT rate Value for IC LIS3DHTR ?

Posted on April 06, 2017 at 08:15for Doing FMEDA I need FIT rate value for IC LIS3DHTRIn data sheet ,reliability data  it is not mentioned.

LSM6DS3 strange values in FIFO

Posted on April 05, 2017 at 11:44I have an LSM6DS3 gyro / accelerometer connected to a Raspberry Pi 3B using i�c. I'm using the internal FIFO to get samples from the gyro and accelerometer. The data is plausible most of the time, however, every now ...

LSM6DS3 Packaging information (Barcode)

Posted on December 13, 2016 at 20:28I have an issue with a batch of LSM6DS3 and I would like to check the chip mark code. I was able to convert the barcode into a code (785320G709QQ) but I couldn't find a place to identify what each number means. Th...

Linux Drivers for lsm9ds1

Posted on April 03, 2017 at 15:47Hi ST Experts,Currently i am working on lsm9ds1 sensor. We are done with hardware connection and we have tested it using sample application using ioctl. In this we are using the polling mechanism. We have to get data...

i didn't obtain licence key to enable the libraries

Posted on April 03, 2017 at 14:25i generated the keys with the OSXLicence wizzard and generated a mail to transmit information ('between lines') and with the nucleo f401re but i did n't received acknowledgement mail.Can you check this , i'll use it ...

STEVAL-IDB007V1, old usb serial fw detected, OLD DTM FW detected

Posted on April 02, 2017 at 12:47Hi All,I am using STEVAL -IDB007V1 development KIT, i installed BlueNRG GI c2.2.2, when i try to connect to the device(click connect), i am getting 2 messages:1-  old usb serial fw detected.2- OLD DTM FW fw detected....

Nav Dev by Associate II
  • 446 Views
  • 0 replies
  • 0 kudos

53L0-SATEL problem

Posted on March 23, 2017 at 13:25I'm having some troubles using the VL53L0X sensor (53L0-SATEL-I1 board); I used the other satellite board included in the x-nucleo-53L0A1 without any problems, but the 53L0-SATEL-I1 isn't working properly; it seems t...

LSM9DS DEN_A/G

Posted on March 29, 2017 at 18:10Hello,How could I enable the DEN_A/G signal?I succeeded to enable the DRDY_M or INT1_A/G signal but I have nothing on this DEN_A/G.Do you have any suggestion?Best regardsMich

Mich1 by Associate III
  • 749 Views
  • 4 replies
  • 0 kudos