MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

[VL53L0X] PerformRefSpadManagement Error

Posted on April 27, 2017 at 11:42Hi, I'm using the VL53L0X satellite with the STM API.For the first time calibration I'm following the calibration flow proposed in UM2039.DataInit() and StaticInit() work well, but after using PerformRefSpadManagemen...

VL53L0X can't change I2C address

Posted on September 27, 2017 at 14:19Hi there,I have one VL53L0X ranging sensor that works fine with the ST library.I performed the sensor configuration and I can read data form sensor.Now I should add a second ranging sensor on the same I2C bus.To ...

Fede Rico by Associate III
  • 1902 Views
  • 1 replies
  • 0 kudos

VL53L0X: Verifying Changed Address

Posted on September 05, 2017 at 22:29I'm using one of these sensors with a nrf52 board. I'm looking for a way to check/verify if the address on one of the sensors is already set to what I want to set it to (before I try to set it, obviously). My ide...

Increasing the range of rc522

Posted on October 05, 2017 at 11:35Hello all, I'm working with the rc522 rfid reader for a project. However the range of rc522 is only about 4-5 inches. I want read range of about 1 metre. I have read about a method to increase the range by connecti...

LIS3MDL reliability data

Posted on October 04, 2017 at 12:02Hello, I'm looking for the MTBF or the failure rate of the http://www.st.com/en/mems-and-sensors/lis3mdl.html3-axis magnetometer .#mems #reliability #magnetometer

LIS2HH12 : How to efficiently record all accelerometer datas ?

Posted on October 03, 2017 at 13:32Hello,I'm using the LIS2HH12 accelerometer for my project.I want to record all the x,y,z datas during 2 seconds without any loss at a high frequency.What is the best way to do that (Which FIFO mode...) ?#lis2hh12 #...

Cannot return in Stream Mode after IT

Posted on April 12, 2017 at 15:51Hi,I'm working on the LIS2DH12 and I have issues when I configure it. I want to use the Stream-to-FIFO mode, and I want INT1 to trigger when one of the acceleration axis is above the threshold. I have configured the ...

H3LIS331DL Configuration Doubts

Posted on March 22, 2017 at 10:40Hi,I'm working with H3LIS331DL MEMS sensor. I read the IC datasheet many times, but I still have some doubts on how to configure it. In particular I ask you: INT_THS register: it is a 7bit threshold while data is a ...

Can i get VL53L0X sensor’s error code table

Posted on September 28, 2017 at 03:48I'm using a pololu's VL30L0X sensor.during checking SNSR'S return value.sometimes I can see the 8190using a searching 8190 means nothing thing in the rangelike this can I get some return Value's meaning exaltlyli...