MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! LIS2DE12 Accelerometer I2C data Reading Problem

Posted on November 12, 2017 at 08:35Hi, I'm working with LIS2DE12 for motion detection. I have configured INT1. Whenever motion is detected I'm reading  INT1_SRC but its value is not changing. It is always same 01101000. Here's the configurations I ...

LSM6DS33 => problem with self test

Posted on November 13, 2017 at 11:16Hello,I recently bought two Pololu IMU03a systems, and both of them gives me negative self test (both accel and gyro). To communication I use I2c protocol.  During the test the device is stationaryCalibration:Rej....

How to get mG from LSM303DLHC

Posted on November 13, 2017 at 19:49I have developed a very simple driver for this sensor. I have a stm32f411ve discovery board which has one included.This is my configuration:PM_LSM303DLHC_config.ctrl_reg1_a = 0x27; PM_LSM303DLHC_config.ctrl_reg2_a...

Bi ribu by Associate
  • 946 Views
  • 1 replies
  • 0 kudos

Problems in reading FIFO for LIS2DE12

Posted on June 09, 2017 at 08:18Hello all,I am configuring LIS2DE12 accelerometer with JN5169 module using I2C. I read the AN3308 application note of LIS3DH and implemented the code accordingly but I am facing the problems in the configurations.I ha...

LIS2DE12 no interrupt and constant acceleration values

Posted on October 09, 2017 at 18:31Hello,Firs of all thank you for your time.I'm currently working with a LIS2DE12 for its great low power current but unfortunately I'm not able to get any useful information from the device. I tried to active an int...

Resolved! LIS2DE12 Accelerometer data bytes

Posted on November 09, 2017 at 22:50http://www.st.com/content/ccc/resource/technical/document/datasheet/group0/72/cb/80/a7/5e/fe/46/9d/DM00153214/files/DM00153214.pdf/jcr:content/translations/en.DM00153214.pdfsays it provides 8-bit accelerometer val...

_legacyfs_online_stmicro_images_0690X0000060MvBQAU.png _legacyfs_online_stmicro_images_0690X0000060MvGQAU.png

Resolved! FIFO Mode of LIS2DE12

Posted on October 21, 2017 at 00:43I am trying read the X, Y, Z values in FIFO mode. I don't understand the reading procedure.Do I need to start reading from FIFO_READ_START and continue reading 6 bytes and then initiate another reading from FIFO_RE...

LSM6DSL FIFO Continuous mode

Posted on November 01, 2017 at 16:11Hello, The app note (pg 98) show an example to FIFO continuous mode.Looking at figure 29 it seem that the FIFO restart filling from F0 ('first' memory location) once read cycle begins.Is this the case? Shouldn't ...

0690X00000608lVQAQ.png

Zero-gauss level on LSM9DS1 (magnetometer offset)

Posted on November 03, 2017 at 13:15We are working with the LSM9DS1 and I would like to know if it is normal to obtain very large offsets for the zero-gauss level, and completely different offsets on different sensors (same PCB design).I previously ...

David M. by Associate II
  • 1680 Views
  • 1 replies
  • 0 kudos

Improvement of Complicated sensor network design

Posted on November 06, 2017 at 08:56 I was working on a project recently and it was the first one which was involved enough to make the sensor networking complicated. In the end, I think the communication was the bottleneck in terms of overall perf...