MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! LIS2DE12 Accelerometer data bytes

Posted on November 09, 2017 at 22:50http://www.st.com/content/ccc/resource/technical/document/datasheet/group0/72/cb/80/a7/5e/fe/46/9d/DM00153214/files/DM00153214.pdf/jcr:content/translations/en.DM00153214.pdfsays it provides 8-bit accelerometer val...

_legacyfs_online_stmicro_images_0690X0000060MvBQAU.png _legacyfs_online_stmicro_images_0690X0000060MvGQAU.png

Resolved! FIFO Mode of LIS2DE12

Posted on October 21, 2017 at 00:43I am trying read the X, Y, Z values in FIFO mode. I don't understand the reading procedure.Do I need to start reading from FIFO_READ_START and continue reading 6 bytes and then initiate another reading from FIFO_RE...

LSM6DSL FIFO Continuous mode

Posted on November 01, 2017 at 16:11Hello, The app note (pg 98) show an example to FIFO continuous mode.Looking at figure 29 it seem that the FIFO restart filling from F0 ('first' memory location) once read cycle begins.Is this the case? Shouldn't ...

0690X00000608lVQAQ.png

Zero-gauss level on LSM9DS1 (magnetometer offset)

Posted on November 03, 2017 at 13:15We are working with the LSM9DS1 and I would like to know if it is normal to obtain very large offsets for the zero-gauss level, and completely different offsets on different sensors (same PCB design).I previously ...

David M. by Associate II
  • 1668 Views
  • 1 replies
  • 0 kudos

Improvement of Complicated sensor network design

Posted on November 06, 2017 at 08:56 I was working on a project recently and it was the first one which was involved enough to make the sensor networking complicated. In the end, I think the communication was the bottleneck in terms of overall perf...

INT1(Programmable interrupt) of L3GD20H

Posted on November 02, 2017 at 14:39Hi Alli will use 'L3GD20H MEMS motion sensor: three-axis digital output gyroscope' in my Project.Pin No 7. which is INT1(Programmable interrupt).Please share me how its pin work. when its generate interrupt.    Th...

Few questions about TOF sensor

Posted on November 01, 2017 at 04:171.VL53L1/VL6180X can work in a dark environment(no Light)?2.  What is the max sampling rate of VL6180X ? can up to 50hz?3.  What is the resolution of VL53L1?Thank you so much.

VL53L1 availability?

Posted on November 02, 2017 at 06:00Is there an approximate date when distributors may start offering this chip?Thanks!

Paul N by Associate
  • 753 Views
  • 0 replies
  • 0 kudos

Resolved! How to wireconnect LSM330DLC with SPI mode

Posted on October 31, 2017 at 08:41This is fundamental question, but I am confusing...Please tell me what I think is right or wrong:To communicate with LSM330DLC on SPI mode, the number of wiring between host and LSM330DLC is 5.1 CS_A2 CS_G3 SCL_A/G...

Resolved! How does FIFO decimation work in ISM330DLC?

Posted on October 30, 2017 at 18:14In FIFO_CTRL3 of ISM330 DLC, you allow the data from both gyro and accelerators to be decimated by the factor in this register. I'm wondering if it is doing an average based on the decimation factor? or is it just ...

gto by Associate
  • 1401 Views
  • 1 replies
  • 0 kudos