MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

hello everyone ,i need help with lis3dsh power waste

Posted on January 12, 2018 at 04:25when i use lis3dsh , i test the power waste is 1.7mA, is more big than the discription in datasheet. the way i use it: the circuit board use STM32F4discovery , i init the gpio ,and then measure the Electric current...

AIS3624DQ WHO_AM_I returning 0XFF

Posted on January 04, 2018 at 13:18the following code i have written for STM32F103C8T6 for interfacing with AIS3624DQ accelerometer. But while checking , when i read register WHO_AM_I (0x0F) it should return me 0X32 default but it is returning me 0X...

LSM6DSL sensor hub with LIS2MDL

Posted on January 16, 2018 at 09:17Hello,I'm using LSM6DSL in sensor hub mode with LIS2MDL, using the example in IKS01A2 I have managed to activate the LIS2MDL and read data from it.My current issue is that I can't put the LIS2MDL in low power mode,...

priven by Associate II
  • 2462 Views
  • 6 replies
  • 0 kudos

LIS3DH ADC function problem

Posted on January 12, 2018 at 13:07Hi, I got a problem in LIS3DH ADC function, we use LIS3DH ADC1 to detect the battery power in our product, but now we found that ADC can't work in the new lot of LIS3DH, the date cod is 8734. And the lot of data co...

Jason Kuo by Associate II
  • 6676 Views
  • 6 replies
  • 0 kudos

VL53L0 API with Nucleo32L0

Posted on January 16, 2018 at 17:08Hi everyone. I'm trying to use VL53L0X satellites with my nucleo32 (STM32L031K6) but i'm having a lot of problems to integrate the API. I'm generating the initial code with STM32CubeMX and importing the project to ...

Resolved! LIS3DSH self-test function

Posted on October 06, 2017 at 16:09Hi all,I am trying to implement the self-test function of the LIS3DSH, but the results I am getting do not agree with the numbers in the device datasheet. Here is my procedure:1) Set -/+2g range and 400 HZ ODR.2) C...

LSM6DSL zero-g level offset accuracy

Posted on January 04, 2018 at 16:28Hi everyone,I'm using the lsm6dsl for acceleration measurement. But I'm getting big stationary offsets and I was wondering is that normal? Here are measurements from 5 different boards and all of them were carefull...

palenkic by Associate II
  • 3208 Views
  • 5 replies
  • 0 kudos

MTBF/FIT rate

Posted on January 12, 2018 at 07:51I need the MTBF/FIT rate for part number STMPE811QTR. Thank you.

LIS2DH: Minimum delay between commands during Self-test

Posted on March 28, 2017 at 17:08Hi,is it possible to know the minimum delay required to wait between register writing during the self-test?I write down my code, to make myself more clearwhile(1) { BYTE xH = 0; BYTE yH = 0; BYTE zH = 0; //HPF disab...

Cesco Gar by Associate II
  • 2204 Views
  • 3 replies
  • 0 kudos