MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

VL53L0X_SetVcselPulsePeriod?

Posted on June 21, 2018 at 19:54is there any information of any type regarding the funktion   VL53L0X_SetVcselPulsePeriod how do i use it in other ways then what is in the API note?

Wrong result from MotionFX

Posted on June 21, 2018 at 14:18Hello,I'm trying to get run the MotionFX library using STM32L4 and SensiBLE board (which is equivalent to Nucleo-L476RG + X-Nucleo-IDB05A1 + X-Nucleo-IKS01A1 + X-Nucleo-CCA02M1).The module for the accelerometer and gy...

VL53L1 Accuracy Issue

Posted on June 19, 2018 at 14:12HiWe have interfaced VL53L1 to STM32L0 EVM board(B-L072Z-LRWAN1).We tested the sensor with a white surface and water in opaque object.The accuracy with white surface are good if the object is below 200cm.If above 200c...

Where to find VL53L1x window cover?

Posted on June 10, 2018 at 20:50I need an outdoor window cover for the ToF VL53L1X. I�m planning to use it as a people detector sensor. I want to put it into an abs plastic case.Here is the module that I obtain from Pololuhttps://www.pololu.com/prod...

Resolved! LIS3DE vs. LIS3DH HW FIFO Handling

Posted on June 11, 2018 at 14:55Hello,we've been using the LIS3DH on a development board and have switched to the LIS3DE for the prototype. We're using the HW fifo feature to batch-read values from the sensor. The LIS3DE is only 8-bit and thus I was...

Resolved! What is the silicon square on the LPS22HB and LPS25HB?

Posted on June 18, 2018 at 11:17In section 10.1 of the datasheet for the LPS22HB the square on top of the package is labelled as 'Sensing area (exposed silicon)', which makes it sound quite fragile.  However I noticed in a recent press release: http...

mart J by Associate II
  • 1645 Views
  • 4 replies
  • 0 kudos

Problem with the basic project of the SensorTile

Posted on June 14, 2018 at 17:13Hi everyone,I've downloaded the basic project of the SensorTile from the St official site, when I try to rebuild with the IAR platform I obtain this error:Error[Li005]: no definition for '__iar_FSin' [referenced from ...

How to do OPC of LPS22HB or LPS22HD?

Posted on June 15, 2018 at 11:36I'm trying to find the opc procedures of LPS22HB or LPS22HD.The datasheet only states you would refer to the pressure offset register.There're no detailed information about opc procedures.Where can I found that?These ...

just4you by Associate II
  • 1977 Views
  • 3 replies
  • 0 kudos