MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LSM303D Interrupt threshold

Posted on June 07, 2018 at 13:20Hi,I am using a LSM303D with a Adafruit Feather M0 and want to detect spikes in the magnetic fields, preferably for all the axes, and want to use interrupts.I have the interrupts working when any of the axes goes abov...

LSM330 vs LSM330DLC

Posted on June 04, 2018 at 14:21HiIs there any comparison table?Best regards.Jokin

IHS1 by Associate II
  • 595 Views
  • 1 replies
  • 0 kudos

BlueCoin logging to SD Card with DataLog

Posted on April 10, 2018 at 14:21Hi,I'm trying the example software for the BlueCoin, also DataLog. The USB streaming of data is working the way it's written in a Start guide. But I'm not moving forward with DataLog on SD Card. I'm going through the...

How to interface X-NUCLEO-IKS01A1 to Nucleo144 L4R5ZI

Posted on June 05, 2018 at 14:15Hi How to interface or bridge up X-NUCLEO-IKS01A1  to Nucleo144 board. I ask this question because the Pin out placing for both the boards doesnt fit as it fits for Nucleo64/32. ThanksPhani.#l4r5zi #x-nucleo-iks01a1 #...

Regarding LIS2MDL Sensor calbration

Posted on June 05, 2018 at 09:38Hello ,     I am working on lis2mdl sensor getting raw data values like below.C5 FF B9 FF 12 00 C5 FFthese values are accurate or not .if values getting correct may i know how to do calibration for that. my pseudo cod...

krish j by Associate II
  • 466 Views
  • 0 replies
  • 0 kudos

LSM6DS33 FIFO watermark interrupt issue

Posted on June 04, 2018 at 23:53Good day everyone!I am trying to use a FIFO watermark interrupt on LSM6DS33 accelerometer. For some reason, the interrupt doesn't happen. Other interrupts (Free-fall, movement, significant motion) work just fine, so i...

How to design a High Speed data logger?

Posted on June 04, 2018 at 15:13Hai, I want to build a data logger attached to an object travel at 3m/s. The requirement is the data logger must capture 74 sensor input (10 bit ADC) at every 3mm along the travel path. Thus in 1 second, the data logg...

Sensor Tile Linear Acceleration

Posted on June 02, 2018 at 10:08Hi ThereI recently got the STEVAL-STLKT01V1 sensor tile evaluation kit. I know that some of the sensors on the sensor tile are able to record linear acceleration (LSM303AGR). I have been looking at the provided exampl...

HTS221 I2C STOPS WORKING

Posted on June 13, 2016 at 07:51Hi, I'm using the HTS221 with STM8L052C6. The communication channel is I2C. I am able to get the humidity data upto 99% RH. but above this after some point of reading the data,the sensor gets hanged and is not recover...

unnati811 by Associate II
  • 1166 Views
  • 4 replies
  • 0 kudos

STM32 Cube and ADXL345 ACC

Posted on May 31, 2018 at 13:46Hi,I am trying to use STM32 cube and ADXL345 ACC using SPI , this is my first time trying , and currently without luck as i am not able to read the accelerometer This is my SPI init code :void MX_SPI1_Init(void){hspi1....