About LSM6D33
Posted on May 16, 2018 at 21:20Hi, what is the bandwidth of the gyroscopes analog anti-aliasing filter?
Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.
Posted on May 16, 2018 at 21:20Hi, what is the bandwidth of the gyroscopes analog anti-aliasing filter?
Posted on May 14, 2018 at 16:11Hello, can you please tell if the temperature sensor on ISM330DLC returns absolute temperature values or the difference values with respect to a reference? Just read a thread (https://community.st.com/0D50X00009XkXfjSA...
Posted on May 16, 2018 at 15:55Hello, i`m trying to get data from X-NUCLEO-CCA02M1 to my NUCLEO-F207ZG vis I2s2 and i2s3, but unfortunetly i have even no I2SX_SCK on my device, what can be wrong ? I set transmission mode to mode master recieve.Tha...
Posted on December 08, 2017 at 06:00 The original post was too long to process during our migration. Please click on the attachment to read the original post.
Posted on May 14, 2018 at 23:33The datasheet mentions accuracy +/- 3.5%, 20%-80% non-condensing and +/-5%, 0%-100%, non-condensing. Is this over -40C to 85C temperature range? Thanks!
Posted on May 11, 2018 at 22:21The LSM9DS1 datasheet lists typical and max supply current for two cases: (1) gyroscopes off and accelerometers and magnetometers active, and (2) gyroscopes active and accelerometers and magnetometers off. I need the ...
Posted on May 12, 2018 at 08:52Dear sir,I want to read X,Y,Z data from LIS3DH. I have gone through the datasheet of the same but still didn't understand what are the commands to access it. So it will be kind of you if you tell me the commands or alg...
Posted on May 12, 2018 at 07:33Hello,Unfortunately, I am having problems with the demo included in the X-CUBE-MEMSMIC1 package for the NUCLEO-L476RG. After loading the precompiled file to the board and attempting to plug it in to a computer via the ...
Posted on May 08, 2018 at 13:21VL53L1x ROI change does different distance measurements Hi, all!maybe someone can explain me why when I change ROI (range of interest) parameter of VL53L1x sensor then I got different distance to the same object (for e...
Posted on May 07, 2018 at 14:31Hi guys, I have some issues to configure the wakeup interrupt on the LSM6DSL. Does one you have already configured this interrupt?