MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LIS3DH operation without controller?

Posted on July 10, 2018 at 01:57Hello, Would it be possible to run the LIS3DH accelerometer without a controller? I know one would be required to program the registers for device configuration, but would it be possible to configure it just once, the...

IIS2DH read temperature

Posted on June 09, 2017 at 12:56I want to read the temperature from IIS2DH over I2CI set the ODR to 1Hzset the BDU bit in Ctrl Reg 4enable the Temerature sensor in TEMP_CFG_REGafter the initialization I read the STATUS_REG_AUX and the value of this ...

control VL53L0X without windows

Posted on July 12, 2018 at 04:51I'd tried to control VL53L0X by Renesas micro computer RX231 with API STSW-IMG005 but the compiler generates many errors. It seems the compiler doesn't support 'windows.h', windows API.Now I am trying to create a new ...

Unable to read the all sensors values at once L475E-IOT01

Posted on April 23, 2018 at 08:37Hi everyone,I am using STM32L475 B-L475E-IOT01 kit. My problem is that it does not give me sensors values at once. I want to get the temperature, humidity, pressure, accelerometer and gyro at once. But it only gives ...

Arduino and X-NUCLEO-NFC05A1

Posted on April 02, 2018 at 21:26Hello!I want to connect the Arduino UNO and http://www.st.com/en/ecosystems/x-nucleo-nfc05a1.html, and I want to know if it is possible. And if yes has anyone already done it?#uno #x-nucleo-nfc05a1 #arduino

M95320 Device Information Page not returning

Posted on June 28, 2018 at 11:54 Hi, I am using the M95320 EEPROM and sending RDID instruction to read the Device Identification page however the device is responding with 0xFF for all 32 bytes on the MISO line. The 2 byte address I am sending is...

0690X0000060LX8QAM.png
dman by Associate II
  • 2836 Views
  • 9 replies
  • 0 kudos

LSM303AGR - how to remove raw data distortion?

Posted on July 02, 2018 at 12:44Hello, erveryoneI have a question about raw data correctness. I read raw data from magnetometer. I reached following results after rotated this around Z axis in horizontal, flat plane, data are expressed in gauss:Red ...

0690X0000060C8QQAU.png 0690X0000060C8aQAE.png

LSM6DS3 spi interface always gives low output

Posted on August 11, 2016 at 13:03I am working on STEVAL-MKI160V1 board which has LSM6DS3 sensor. I want to interface board to AARDVARK I2C/SPI adapter using which I can generate I2C/SPI signals to the sensor. I connected sensor board to adapter, us...

n239955 by Associate
  • 750 Views
  • 3 replies
  • 0 kudos

How to configure a STM32CubeMX project for a STM32F769I-Disco board to use only the MEMS Mics and the out audio jack ?

Posted on July 06, 2018 at 18:19Hi, I am currently working on a STM32F769I disco board and I would like to create a minimalist project (i.e. I only want what is necessary to my project) I want to use the MEMS Mics to playback directly on the jack ou...

Resolved! LSM9DS1 Magnetometer Temperature Compensation

Posted on February 13, 2017 at 15:59What does the TEMP_COMP bit in CTRL_REG1_M of the magnetometer do?  Do the offsets need to be programmed for it to work?We are seeing up to 10 degree heading variations when moving the temperature from 10C to 30C,...