MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LSM6DS3 problem

Posted on July 19, 2017 at 05:24Hi, i am working with LSM6DS3 sensor, this is the first time i work with type of sensor. i am trying to read out gyro z data, but it very noise when sensor is immobile.Here is my log:-120-93-127-69-79-41-85-97-72-57-8...

ice by Associate II
  • 937 Views
  • 3 replies
  • 0 kudos

Resolved! LSM6DSL does not behave as expected in FIFO continous mode

Hi Everyone,I am Using the L6MSDL chip for my application (connected to a STM32L4) in FIFO Continuous Mode and I am having some troubles understanding the FIFO pattern that we can read in FIFO_STATUS3 register. I configured the LSM6DSL The following ...

How is the INT1_THS scaled on the LIS3DH sensor?

I try to use the LIS3DH as a fall sensor in an security device for elderly people. I want to use a more elaborate detection method than just using the free fall interrupt and therefore I try to define a fall as first a free fall interrupt and then an...

PHand by Associate
  • 1104 Views
  • 2 replies
  • 0 kudos

Resolved! Typo in datasheet for LPS25H?

Hi.I wonder if it is possible to disable the I2c interface via CTRL REG2?in 7.7 in the datasheet it seems to be possible, but specification for bit 3 seems strange:[3] I²C enable (0: I2C enable;1: SPI disable)Is above this correct in the datasheet? i...

FFrid by Associate
  • 774 Views
  • 2 replies
  • 0 kudos

TOF Sensor regarding

Hello sirGreetings !!!!!We have selected your TOF Sensor part number vl5l0x this sensor detect range 1.2 Meter in the White background but our requirement is TOF Sensor detect range in any color of the object up to 2 meters.so please share the TOF se...

hjani by Associate
  • 462 Views
  • 0 replies
  • 0 kudos

LIS2DE12TR: Trying to set up 4D/6D mode to trigger an interrupt

The datasheet for LIS2DE12TR is utterly confusing. It is missing any kind of flowchart for how the device operates in 4D/6D mode, or how to even set up registers correctly to enable these modes without conflict. Moreover, the registers are describ...

APast by Associate
  • 581 Views
  • 1 replies
  • 0 kudos

LIS3DE reset w/o supply reset

We're using a LIS3DE in our project wired up to the MCU as following:So we're using I2C for communication and have access to both INT pins, but not to the reset line and neither is there a mechanism to hard-reset the accelerometer.During development ...

0690X000006BwSnQAK.png

Resolved! Any application software for STEVAL-WESU1 board

Posted on April 20, 2018 at 16:16Hello Experts,Recently I bought the STEVAL-WESU1 board and able to read the sensor data using android application.My requirement is to connect this wearable platform to other ARM board (raspberry pi board), raspberry...