MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

VL53L1X range readings not accurate after 200cm

We are testing VL53L1X Time of Flight Sensor with STM32L072(B-L072z-Lrwan) controller. Within 200cm the range measured by sensor is accurate. After 200cm we are getting a lot of variation in the range is measured by the sensor. We have to change the ...

Resolved! LSM303AGR can't enable temperature sensor

I am having a problem when initializing temperature sensor on LSM303AGR. To simplify everything for a test I am using direct commands. Writing 0xC0 to register 0x1F and then reading back register 0x1F results in 0x00 reply instead of 0xC0. Why is it ...

MHuk by Associate II
  • 692 Views
  • 1 replies
  • 0 kudos

LSM6DSL - values not correct

Hi :) i m using LSM6DSL accelometer . i My sensivity is -2g/+2g. I have 16 bit (65535 values ) . Well, when i take values, i have values as: 65,423- 64,912 - 16,076325 - 61,613 - 58448 I dont undestand this value. I think 16,076 is 1 g...

EWARM problem with compiling of MEMS1 example projects

I am tring to compile and run the examples of IKS01A2 sensor evaluation board (on STM32F401RE).after buil there is no errors but I getting this msg in the debug log running periodicaly:Do someone knows how to fix this problem? I tried all my ideas.....

ALesh by Associate II
  • 640 Views
  • 2 replies
  • 0 kudos

VL53L0X single ref calibration error

Posted on December 04, 2017 at 15:52 Hello, i want to use the VL53L0X sensor with an ARM processor. For that purpose I took the Pololu Arduino library, rewrote the i2c part and everything worked fine. My problem with the Pololu librays is that...

VL53L1X GUI Connection failure

Hello,I am using Windows 7 Ultimate and have the same problem that community member dconrad has already described very well. (see link).In addition, I noticed the following:When the GUI is runing, the red glowing double LED LD1 on the board, flashes ...

Markus1 by Associate
  • 513 Views
  • 0 replies
  • 0 kudos