MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

how to simulate Sent protocol ?

Hello everybody,I wanted to simulate the Sent_Protocol with a STM32 µC or simulate it as if I had a sensor. and present this with oscilloscope. Now the signal should be like a normal PWM Signal look like. I really do not know how to generate this par...

Samuel1 by Associate III
  • 2270 Views
  • 0 replies
  • 0 kudos

L3GD20H can't set Low_ODR bit

Hi everyone,I am using a L3GD20H gyro on a custom board. I am successfully talking to it and have been able to set the following registers to values:CTRL1_reg: 0x0F (power enabled, all axes enabled)CTRL3_reg: 0x08 (INT2 set for data ready signal)CTRL...

MMacL.12 by Associate
  • 1804 Views
  • 3 replies
  • 0 kudos

Wrong accelerometer value from LIS2HH12

Hello!Have bought the STEVAL-MKI183VI for the LIS2HH12 device.The device are enabled for all direction by wrinting the following to the ctrl1 register   regData.ZEN = 1;  regData.XEN = 1;  regData.YEN = 1;  regData.ODR = ODR_100_HZ;  regData.BDU = 1;...

OChri by Associate
  • 688 Views
  • 0 replies
  • 0 kudos

Problem while receiving data from the MEMS microphone.

I am using the STM32F407 discovery board and Wolfson pi audio interface. I have a problem in analysing sample values received from MEMS microphone.I wanted to plot the data sensed by the MEMS microphone, which is just sensing the surrounding environm...

rrach by Associate II
  • 777 Views
  • 0 replies
  • 0 kudos

Resolved! Accelerometer for use in boat engine

I have been asked to embed an accelerometer into the engine control module. It would normally be used when the engine is not running to determine static angle with respect to gravity; low G, angle sensor. However, once the engine starts running there...