MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! LSM6DS3 + LIS3MDL calibration

Hello, Our teams is making a proof of concept about dead reckoning using a STM WESU board. The goal is to get pedestrian position onyl using ACC/GYR/MAG for a short period of time and small moves.First results in certains conditions are pretty good. ...

pierre63 by Associate II
  • 1808 Views
  • 7 replies
  • 1 kudos

Resolved! LSM303DLHC software

Hi ThereWhere I can find some source files for LSM303DLHCI see some ref.links there, but right now they pointed to non-existed pages on github :( Or I miss somethingAlso I found this link https://github.com/STMicroelectronics/stm32-lsm303dlhc but it ...

LoMo-MoMo by Associate II
  • 1200 Views
  • 8 replies
  • 5 kudos

LPS22HBTR sensor data error.

Dear ST/Forum,Your attention would be much appreciated for a technical enquiry.We are using the LPS22HB pressure and temperature sensors in some electronics for an experiment that will be onboard the International Space Station (ISS) in orbit later t...

DuncanR by Associate II
  • 1041 Views
  • 2 replies
  • 0 kudos

Resolved! Sensor Recommendation for Vibration and Motion Detection

Hi, We are developing a product/device that is mounted on a machine/vehicle that generates vibrations when in the ON state. We need a sensor that can 1.. Detect vibration start and stop while the device is stationary, with good accuracy, to determine...

Jayk by Associate
  • 857 Views
  • 6 replies
  • 0 kudos

Resolved! FSM double tap

Hi, I'm trying to implement the tap and double-tap function in the FSM tab. Is it possible to achieve this at an output data rate of 26 Hz? 

SamuPre by Associate
  • 1236 Views
  • 1 replies
  • 1 kudos

Continuously varying output from MEMS Gyroscope

We are using the X-STM32MP-GNSS2 (with the STM32 discovery board DK2), which has ISM330DHCX IMU. The accelerometer readings seem fine from the IMU, but the gyroscope gives enormously high and varying readings even when we are stationary. See below th...

STEVAL-PROTEUS: Serial Monitor over Micro USB

Hi all!I've recently started working on a fault classification model utilizing the proteus1 board and the NEAI studio suite. I'd ideally like to set up a serial datalogger via the onboard micro USB to both obtain and display readings, alongside bench...

Haze by Associate II
  • 1208 Views
  • 2 replies
  • 0 kudos