MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! SensorTile.Box PRO and STEVAL-MKI168V1

Hi, I have an evaluation board STEVAL-MKI168V1 with the sensor IIS2DH. I was hoping to plug it into the DIL24 connector of the SensorTile.Box PRO and be able to see the sensor's output using the MEMS Studio. This does not seem to be the case. Can som...

msv by Associate II
  • 1580 Views
  • 3 replies
  • 0 kudos

LIS2MDL, MAGNETOMETER

Hello, I am using the LIS2MDL development kit. I have two questions. When I measure with two development kits in the same environment, I get different values.Both are 5 cm away from each other and there is no factor that will disrupt the magnetic fie...

AlpoTemi by Associate II
  • 2084 Views
  • 6 replies
  • 2 kudos

Compensate for Temperature Effects on IIS3DWB

I’m currently developing a vibration meter device and using the IIS3DWB accelerometer. I want to ensure that my acceleration data is as precise as possible. I’ve read that temperature can affect the accelerometer’s performance, so I’m looking for adv...

LIS3DH tilt angle and shock interrupts + ADC

Hi, First of all, I'm not proficient with embedded C, but I would appreciate any input from you that I could feed to ChatGPT. I've been trying to have the codes generated, but they simply would not produce what I wanted. So I have a LIS3DH IMU connec...

MEMS elements inside an accelerometer (LIS2DH12) get stuck

I have a device which uses an accelerometer (LIS2DH12) to trigger a wake up upon movement. Now I have a few samples on my hand, where this wake-up does not work. The design, configuration, interrupt, etc of the parts work (as validated by other ident...

CF3nXftw by Associate II
  • 1193 Views
  • 2 replies
  • 0 kudos

Resolved! LSM6DSV80x SLFP game rotation vector, and timestamp to fifo

Hi there, I'm trying to program LSM6DSV80x to read sensor values in -500Hz for a certain period of time and send them for process (thus no realtime process, but need timestamps).  The sensor values include xl, hg_xl, gyro, and also Game rotation vect...

LIS2DH12 configuration

Hi, I am, working with LIS2DH12 and I want to detect some variations of Z axis.I don't need to detect accelerations just variations of its current positions over my threshold. My current configuration is the following. CTRL1 (0x20) -> 0x17CTRL2 (0x21...

P M by Associate III
  • 1197 Views
  • 1 replies
  • 0 kudos