MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! LSM6DS3TR Obsolete Drop-In-Replacement

Hi All,   I am working on a design that has been working for years. Now we wanted to design a revision of the PCB with the LSM6DS3TR but sadly it became obsolete and I can't find it back on the website of ST.Could the LSM6DS3TR-C be a Drop-In-Replace...

STEVAL-STWINKT1 with ST MEMS Studio is not working

I am having STEVAL-STWINKT1 to be interfaced on USB channel for ST MEMS PC application.I have flashed DATALOG2_Release.bin in eval kit.I can get the ST MEMS PC Application showing the vibration sensor analysis graph. See attached.However, the issue I...

mdalal_0-1749708646028.png
mdalal by Associate III
  • 2268 Views
  • 7 replies
  • 0 kudos

LSM6DSV32X - understanding I3C DAA

Hello ST Team,I am curious to know how LSM6DSV32X Accelerometers sensor communication takes place.So, basically what I am trying to understand here is when Master assigns some dynamic address to LSM6DSV32X Accelerometers sensor, then where exactly th...

soukum by Associate
  • 927 Views
  • 2 replies
  • 1 kudos

STEVAL-STLKT01V1

Good morning, I am programming a SensorTile using the STEVAL-STLKT01V1 expansion kit, and when I flash the program to the device, I encounter the following error:Break at address "0x8000270" with no debug information available, or outside of program ...

Precise temperature measurement with LIS2DW12: Calibration?

我想使用 LIS12DW12 来准确测试环境温度。我应该用什么方法校准芯片的准对,否则这个芯片不能准确测量温度?有没有关于他的实验错误的数据?Google translation:I want to use LIS12DW12 to accurately test the ambient temperature. How should I calibrate the chip, otherwise the chip cannot accurately measure the temperatur...

Resolved! Is LSM6DSL zephyr driver compatible with LSM6DSR ?

Hi, I am trying to create test the STEVAL-MKI194V1 for a test vehicle, which has LSM6DSR. However, I do not get an initialization response from it using the Zephyr device tree. So, I did a test (without the DSL driver) with the spi shell which gives ...