MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! RoHS certificate and material declaration form

Hi I would like to get HTS221TR materials declaration form.HTS221TR---------- SENSOR / HUMIDITY/TEMPERATURE / 6-VFLGA / SMD //***Edited by Moderation*** - please do not post sensitive information such as physical or email addresses in the community.

SSuar.1 by Associate II
  • 6074 Views
  • 5 replies
  • 0 kudos

Hi everyone, I want to connect ADXL355 accelerometer sensor with stm32F407 mcu using I2C but, there is no any response from the sensor. Can anyone help me? Thanks...

 ADXL355_Result ADXL355_Init(I2C_HandleTypeDef* I2Cx,ADXL355 * DataStruct, ADXL355_Device DeviceNumber, ADXL355_Accelerometer AccelerometerSensitivity){ uint8_t WHO_AM_I = (uint8_t)ADXL355_DEVID_AD ; uint8_t temp; I2C_HandleTypeDef* Handle = I2Cx; /*...

0693W000006Fj6DQAS.jpg
MHass.2 by Associate III
  • 3232 Views
  • 5 replies
  • 0 kudos

LIS2DW12TR accelerometer sensor is used in the current project for detecting the events such as, MOTION detection Tampering detection(single tap with high threshold) when i am enabling both the detections given above, only motion event is detected.

can i know why this observation is observed?enabling all the event INTR's, according to the event occurred corresponding event INTR should be raised, but in my case only single tap event is not observed, can you please take this as a high priority c...

Mnago.1 by Associate II
  • 1244 Views
  • 1 replies
  • 0 kudos

Resolved! Exact measurement position of LSM303D?

Hi, i would like to know where exactly at the magnetic sensor (LSM303D) the magnetic field is measured.We want to locate the exact position of magnet using multiple of these sensors, there for need to know where the value in the sensor is measured?

TScha.2 by Associate
  • 1192 Views
  • 1 replies
  • 0 kudos

Resolved! X-CUBE-IKA02A1 software download

Hello, I'm no longer able to find the X-CUBE-IKA02A1 package on the ST site. I see that the status says it's active, but the software download section states "No data available in table".Could you point me to where I can download the package, I got a...

ADonc.1 by Associate II
  • 1437 Views
  • 2 replies
  • 0 kudos