MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Problems with AFS tool on MEMS Studio -- bad data?

Tools/Software/etc:SensorTile.box PRO with DATALOG2_Release firmwareSTBLE Sensor app (to trigger data collection)hsdatalog_to_unico.pyMEMS Studio v1.4.1Ubuntu Linux 24.04I watched a handful of webinars and read through tutorials related to the LSM6DS...

Screenshot from 2024-12-03 12-51-46.png Screenshot from 2024-12-03 13-38-06.png
rbmarcus by Associate II
  • 5303 Views
  • 12 replies
  • 2 kudos

BLE + Vibration Detection

I am trying to build a project to detect vibration using STEVAL PROTEUS 1 (STM32WB5MMG, ISM330DHCX and BLE SENSOR). Unfortunately my sensor and BLE does not initialize despite 0 errors.I have used custom BLE Template. I have initialized sensor code i...

RB4 by Associate II
  • 1190 Views
  • 7 replies
  • 0 kudos

Receiving data from ASM330LHHXG1 sensor with intterupt

 I am trying to collect accelerometer, gyroscope, and temperature data from the ASM330LHH IMU sensor via SPI by timestamping the exact moment the data is generated. I have connected the INT1 pin of the sensor to the STM32H735RGV6 microcontroller’s PB...

yrnzdn by Associate
  • 694 Views
  • 2 replies
  • 0 kudos

Resolved! ISM330BX SFLP drift

Hi everyone,I’m developing an application that tracks the path of a device using the ISM330BX IMU and sensor fusion. I’ve based my implementation on ST’s GitHub example for sensor fusion, and the rotation outputs appear to respond correctly when I mo...

Leo0n by Associate
  • 649 Views
  • 1 replies
  • 0 kudos

Conneting STEVAL-55G1MBI PCB4189D to SBC

Hi, I have a compulab SBC (UCMiMX8Mplus sbev) it is a dev kit. I am connecting the STEVAL-55GMBI to the board with the edge connector with our custom board. It is connected to the MIPI-CSI2 connection. I have build the vd55g1 driver with the kernel a...

rjoshiIntero_0-1752763629069.png

ISM330 Max Steady State Acceleration

Hello,What is the maximum sustained long term acceleration that the ISM330 can handle before ruining the sensor?I see in the datasheet that the maximum acceleration for 0.2ms is 20,000 G, but I would like to know if it can handle a sustained 100G acc...

BrandonM by Associate II
  • 426 Views
  • 1 replies
  • 0 kudos

IMU acceleration reaching the limits of the sensor.

Hello,I have a case where my IMU (ISM330) can see peak accelerations above the 16G limit.How does this effect the output of the sensor?Could this cause aliasing of my data or would it just cause me to see a lower amplitude?Thank you! 

BrandonM by Associate II
  • 676 Views
  • 1 replies
  • 0 kudos

Resolved! datapro 1 pack is corrupt

 Can someone please provide a working download file for "STM32Cube function pack for STEVAL-PROTEUS1 sensor datalog and file transfer over BLE and USB"?The ZIP-File Version is corrupt.It cannot be extracted neither on Windows, Linux or Mac.Thank you....

RB4 by Associate II
  • 869 Views
  • 1 replies
  • 0 kudos