MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! AIS2120 Accelerometer Sensor

I'm encountering many issues while using the AIS2120 accelerometer sensor and would greatly appreciate your assistance. Thank you very much!After the sensor is powered on, a series of initializations (default configuration) are performed, then it ent...

微信图片_2025-10-10_105353_532.png
Yz2 by Associate II
  • 894 Views
  • 5 replies
  • 3 kudos

Resolved! STHS34PF80 – How to achieve 4 m detection range on Linux

I am using the STHS34PF80 IR presence/motion sensor on a Linux platform . According to the datasheet, the sensor can detect human presence up to 4 m (for a 70×25 cm² object).Currently, my configuration is as follows:echo 1 > /sys/bus/i2c/devices/3-00...

jeena by Associate
  • 496 Views
  • 1 replies
  • 0 kudos

Resolved! AIS2120 CRC and ​​workflow​​

Could anyone give me some advice on debugging the AIS2120 accelerometer sensor? I've included my CRC check function above, as well as the data sent and received via SPI, but I still can't read the correct sensor ID. Thank you very much for your help!

wechat_2025-09-30_123024_833.png wechat_2025-09-30_123322_374.png 微信图片_2025-09-30_111851_590.png
Yz2 by Associate II
  • 559 Views
  • 2 replies
  • 0 kudos

Resolved! AIS2120 CRC

Is this the correct way to calculate the CRC check code?

Yz2 by Associate II
  • 1911 Views
  • 2 replies
  • 0 kudos

Resolved! MotionEC_Initialize generates an error when it is called

Hello,It seems that the library MotionMC_CM7F_wc32_ot_hard.a is missing the called function, here the error :c:\st\stm32cubeide_1.6.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.9-2020-q2-update.win32_2.0.0.2021053...

AMais.1 by Associate
  • 4571 Views
  • 5 replies
  • 0 kudos

Resolved! iis3dwb issue while capturing data max data-rate

Hi,I am trying to capture data from the IIS3DWB sensor at its maximum rate and save it into a buffer of length 8192 (due to internal RAM limitations). I'm using SPI with DMA to interface with the sensor. However, I'm not able to capture the data corr...

Resolved! LSM6DSL: Clarification of CTRL1_XL Register description

Hi ,We need a clarification in the register values of LSM6DSL for configuring g values. Is this the correct values or is it a printing mistake where 16g is given as 01 ,should'nt this value be allocated to 4g .It would be appreciated if you can kindl...

Screenshot 2025-08-13 113214.png
Gouri_k by Associate
  • 688 Views
  • 3 replies
  • 1 kudos

LIS2DU12TR accelerometer

Hi,I am trying to use the LIS2DU12TR's low address that is 0x18 but I keep on encountering issues with not able to read WHO_AM_I and the accelerometer does not work. Can anyone please help me with this?Also, does it support 100kHz I2C bus?Thanks.

PE4A by Associate
  • 2908 Views
  • 3 replies
  • 0 kudos