MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Tilt compensated heading using LIS2MDL and LSM6DSL

Hi,In one of our projects we have to use the accelerometer LSM6DSL, and magnetometer LIS2MDL. The tilt-compensated magnetic heading have to be computed in accordance with the values read from these sensors. We have the respective EVKs connected to ou...

0693W00000LvvSeQAJ.png

Hello! I am currently working with an LSM6DS0 IMU (3D accelerometer + 3D gyroscope), and I would like to use the embedded FIFO in Continuous mode. I have a question regarding the sequence of the samples in the FIFO and what is the proper way to read them

As far as I can understand from the datasheet, the FIFO is shared and there is no guarantee in the sequence of the samples. For instance, accelerometer and gyroscope samples can be interleaved (e.g. first 2 samples are 3-axial accelerometer measureme...

PMylo.1 by Associate II
  • 2131 Views
  • 3 replies
  • 0 kudos

LPS33HW - i2c connection

Hi Guys, i have connected the LPS33HW sensor to my circuitPython code. i have also added another sensor on the same i2c peripheral (bus). one is addressed 0x5d (original), the other i changed the address as advised to 0x5c. however when i run both se...

sadam.11 by Associate
  • 1088 Views
  • 1 replies
  • 0 kudos

How to get actual sampling rate of MEMS accelerometer output ?

I have observed from the FFT that MEMS accelerometer output do not provide correct peak frequency (frequency at max. amplitude). There are some references that talk about variability of sampling rate of MEMS accelerometer. What are the different ways...

AShri.2 by Associate
  • 1193 Views
  • 1 replies
  • 0 kudos