MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Need a help in picking a sensor

Hi,I need an accelerometer sensor that generates an interrupt on the acceleration, Let's say that the acceleration always is 9.8, it'll just generates an interrupt on 11 for example.Because all the sensor that I've tested just generates a specific in...

LSM303AGR Calibration

Hello everyone, I'm contacting you today in order to understand my error during the calibration of my LSM303AGR sensor located on a PCB. The ultimate goal is to create a compass with tilt compensation but I try to get a good precision with magnetomet...

Aquatwix1_0-1740583867072.png Aquatwix1_1-1740584081813.png
Aquatwix1 by Associate II
  • 2590 Views
  • 7 replies
  • 1 kudos

Resolved! Trying to avoid hit or touch detection

I am using the sensor LIs2DH, and I've read the datasheet and tried multiple values and manipulations of its registers.Now I want to use the sensor should be on a car and detect when will the car move.the problem I'm facing that it generates an inter...

abduuu by Associate II
  • 431 Views
  • 1 replies
  • 1 kudos

LSM6DSO freeze and doesn't respond

Hello,  I use LSM6DSO with my stm32L476. I use I2C 100kz with 10k pull up resistor. The LSM6DSO is next to the STM32. I use INT1 with wakeup parameter to indicate the movement and wake the STM32.I have a problem, sometimes the LSM6DSO freeze. There i...

Aurelien3_0-1760070157866.png Aurelien3_1-1760070208989.png Aurelien3_2-1760070249380.png

Resolved! AIS2120 Accelerometer Sensor

I'm encountering many issues while using the AIS2120 accelerometer sensor and would greatly appreciate your assistance. Thank you very much!After the sensor is powered on, a series of initializations (default configuration) are performed, then it ent...

微信图片_2025-10-10_105353_532.png
Yz2 by Associate II
  • 892 Views
  • 5 replies
  • 3 kudos