Resolved! ISM330DLC - filter attenuation in stop band/ order of the filters
Hi,I would like to know what is the stop band attenuation of LPF1 and LPF2 for the sensors ISM330DLC & IIS2DLPC. Thank you!
Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.
Hi,I would like to know what is the stop band attenuation of LPF1 and LPF2 for the sensors ISM330DLC & IIS2DLPC. Thank you!
AN5296Application noteASM330LHH: automotive inertial module digital 3-axis accelerometer and digital 3-axis gyroscope3 Operating modes”To guarantee proper power-off of the device, it is recommended to maintain the duration of the VDD line to GND for ...
Hi, I am working on the LIS2DH12, I have a problem to the appearance of acceleration data. I'm using full scale of +/- 2g and ODR of 400Hz. When the resolution is either 10-bit or 12-bit, only even number acceleration data is read(all x/y/z axis)....
Hello,I have a requirement to log the data from evaluation board STEVAL-STWINBX1 to cloud. I have created Azure IOT hub and while initiating the cloud logging from the app i was unable to successfully connect to the created IOT Device created in azur...
I am looking for information about iNemoEngine sensors in the latest STMicroelectronics HAL for Android.I successfully integrated the STMicroelectronics HAL framework into Android 11. I am using the LSM6DSOTR gyroscope/accelerometer and the LIS3MDLTR...
Hello ST Community,I am currently working on integrating the LSM6DSV16X accelerometer with an STM32H7 series MCU over I²C. Our main goal is to detect the tilt angle of the system. Hardware SetupMCU: STM32H7Sensor: LSM6DSV16X (mounted on a custom boar...
hello , i am using lsmds0 sensor with nxp board below is the section of my code int main(void) { /* Write your code here */ Clock_Ip_StatusType clockStatus; clockStatus = Clock_Ip_Init(&Clock_Ip_aClockConfig[0]); Siul2_Port_Ip_Init(NUM_OF_CONFIGU...
I have a question regarding the absolute maximum ratings of the ASM330LHH.In the datasheet, the Vin rating lists “(including CS, SCL/SPC, SDA/SDI/SDO, SDO/SA0)”.Does this voltage range also include any overshoot and undershoot on these pins?Additiona...
I connected STEVAL-MKI236A and STEVAL-MKI109D and confirmed that the IMU information comes from Mems studio and Unico.My final goal is that this IMU value is output in serial communication.I want to read the output IMU 6-axis information through pyth...
I could successfully operate the X- NUCLEO IKS4A1 in the MEMS Studio with the default sensor selection on the board. However, when I tried to select the LSM6DSV, which is connected on the DIL24 socket of the X-NUCLEO IKS4A1 board, for the accelerome...