MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LIS2DW12 Bias issue

Hi MEMS experts,I am using LIS2DW12 to measure the movement with very rough distance.I tested it by measuring the X-axis only, but it seems to be biased to positive direction.I mean, Moving it to the positive direction : it starts having the + accele...

IIS2MDC read X,Y,Z, temperature via I2C - separately or together ?

I have the IIS2MDC along with LSM6DSL accel / gyro on a board with stm32L451 uC.Accel / gyro work fine. uC reads status byte then if any axis has new data ready it reads all from temp to accel (0x20-0x2d) in 1 ST hal fn call multi byte read: HAL_I2C_...

CClen by Associate
  • 2609 Views
  • 2 replies
  • 1 kudos

What's the best way to complete self-test on ASM330LHH?

I have followed the description in <an5296-asm330lhh-automotive-inertial-module-digital-3d-accelerometer-and-digital-3d-gyroscope-stmicroelectronics.pdf> to write self-test code, but the Accelerometer and Gyroscope's data is still not in the correct...

Xie1 by Associate
  • 1348 Views
  • 1 replies
  • 0 kudos

X-nucleo-VL53L8A1 not working with nucleo-f401re and GUI

X-nucleo-VL53L8A1 not working with nucleo-f401re and GUI,when i connect vl53l8 expansion on Nucleo-f401re ---LD1 blinks red and green...also com port shows in device manager but vl53l8 GUI does not show/detect com port

imdc by Associate II
  • 5089 Views
  • 8 replies
  • 0 kudos

VL6180X library's registers

Hi! I'm using the VL6180X with several libraries for a specific application. However, I have noticed that most of them configure some registers that are not detailed in the manufacturer's datasheet. Therefore, I would like to know what these register...

CRodr.7 by Associate
  • 1747 Views
  • 2 replies
  • 0 kudos