MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LIS3DH读�?�FIFO为空 LIS3DH reads FIFO as empty

设置 ODR400HZ�?范围 2g�?�?�用 FIFO 并�?置�?模�?。读�?��?个寄存器的�?置没有问题。数�?��? 5 毫秒读�?�一次,FIFO �? time_ src=0x20 读�?�一次。

jzhon.3 by Associate
  • 1225 Views
  • 1 replies
  • 0 kudos

SensorTile.box: Send data/text over Bluetooth to be displayed on PC.

Hi, I have created a machine learning model using STM32Cube IDE and would like to print out the results of the model on the PC using Bluetooth. I am using the SenorTile.box (STEVAL-MKSBOX1V1) with the SPBTLE-1S Bluetooth module.I am currently printin...

Bxy by Associate II
  • 1340 Views
  • 0 replies
  • 0 kudos

STEVAL-MKI109V3 and STEVAL-MKI197V1 IMU data rate to 6667Hz

Motherboard: STEVAL-MKI109V3 (STM32F401VETX)IMU board: STEVAL-MKI197V (LSM6DSOX)​Hello, I have ran into trouble setting the LSM6DSOX data rates of the XL and GY to 6667Hz in a custom STM32 project. The data is still fetched at a lower rate of around ...

vv.tl by Associate
  • 1787 Views
  • 2 replies
  • 0 kudos

How to to do GET and POST request with a Steval stwinkt1.

Hi, i'm trying to do GET and POST request with a Steval stwinkt1. The board is connected to the wifi using wifi.h librarie. Currently I connect the board to wifi. Then I send my Get request with the "WIFI_SendData" functionI store the response in a "...

LMesn.2 by Associate
  • 1342 Views
  • 0 replies
  • 0 kudos

Resolved! Powering LIS2DS12 sensor with 2.5 volts

by some mistake, we have a large batch of boards with LIS2DS12 sensor and STM32G030F6P6 mcu powered with 3.3 volts. but the maximum voltage for LIS2DS12 is 2.0 volts, and absolute minimum voltage for STM32G030F6P6 is 2.0 volts. so we tried to adjust ...

CZorg.1 by Associate II
  • 1478 Views
  • 1 replies
  • 0 kudos