MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

IIS3DWB temperature sensor offset

HelloIn the IIS3DWB datasheet, it is said that the embeddeed temperature sensor offset can vary within a [-15°C : +15°C] range.Does that mean that the reading from OUT_TEMP_H/L can vary within [-256*15 LSB : +256*15 LSB] at 25°C ?Having tested 2 chip...

pb38 by Associate II
  • 7008 Views
  • 12 replies
  • 0 kudos

Resolved! LSM6DSR is never setting XLDA in status reg.

I am trying to validate a new board layout and am looking for the minimal configuration to read accel data.I'm using SPI.  When the WHO_AM_I register of the LSM6DSR is queried, the correct response of 0x6B is returned.I take that as validation of the...

Resolved! IIS3DWB bandwidth

Hi,The LPF2 filter on the IIS3DWB can set the cutoff frequency to ODR/4, ODR/10, ODR/20, etc. Figure 6 in the datasheet "Frequency response with LPF2 enabled" shows the bandwidth when LPF2 is set to ODR/4 to be 5.6 kHz. Is this correct? ODR/4 would...

SDiSt.1 by Associate
  • 2942 Views
  • 4 replies
  • 2 kudos

LIS3DH noise while access with I2C

Hi,It seems that accessing the i2c bus add noise to acceleration values read by the LIS3DH. The graphic represent 270 X,Y,Z 10bit samples read at 1344KHz. The FIFO is enable and a watermark level interrupt of 28 is set. At each interrupt, I'm doing a...

leca_0-1694529572520.png leca_1-1694530257485.png
leca by Associate
  • 3034 Views
  • 4 replies
  • 0 kudos

Resolved! LSM6DS3 returning Register address instead of value on most registers

I have multiple LSM6DS3 (with SH SMD markings) and all of them show the same strange behavior.The chip is soldered to a breakout board that is set up on a breadboard. And is connected to the MCU breakout with 20 cm jumper wire.1. When I read a regist...

Maglog by Associate II
  • 3435 Views
  • 6 replies
  • 1 kudos

ST LSM6DS3TR-C Gyro LP Filter

The LSM6DS3TR-C datasheet "Gyroscope LPF1 bandwidth selection" table mentions BWs for 800Hz, 1.6kHz, 3.3kHz and 6.6kHz ODRs. In the same datasheet, the "Gyroscope ODR configuration setting" table lists ODRs of 12.5Hz, 26Hz, 52Hz, 104Hz, 208Hz, 416Hz,...