I'm busy debugging the RF conditions around my LoRaWAN installation.I get a lot of variance in both RSSI and SNR (+-10dB/+-6dB) and am trying to find it's source.In the absence of an SDR and other equipment, is it possible to read and report RSSI an...
Between Board 1 and Board 2 data exchange should be done through LoRa and data exchange between Board 1 and PC should be through USB. It would be very helpful if someone help with this.
I am using P-NUCLEO-LRWAN3 and I have re programmed the sensor board (NUCLEO-L073RZ + LRWAN_NS1) using the STM32CubeExpansion_LRWAN_V2.1.0.I am getting TxTimeout and JOIN FAILED and I can’t execute any AT commands?
I bought the P-NUCLEO-LRWAN3 STM32 Nucleo starter pack for LoRa and it says that if the NUCLEO-LO73RZ board's serial number is within a certain range, which it is, the board must be updated with a new firmware before use. However, the link provided o...
Hi everybody,I have to problem with LoRaWan EU868 certify in Ukraine, specifically as follows:I am using ABZ module as CMWX1ZZABZ-091 to develop product, and I set ABZ module such as:+ firmware based on source code en.i-cube lrwan v1.3.0+ used Lora m...
Hi stm, We are currently reviewing the lora function based on sx1262 semteck chip.I have NUCLEO-L476RG and NUCLEO-L073RZ ref board. It also has an sx1262 Evaluation board that can be attached to the ref board. The NUCLEO-L476RG board has a flash o...
I have an application taht works fine when I power the board from USB ST-Link, but it does not work when powered by battery. LD7 lights up, but no other LEDs. My app turns some on immediately.When powerded by USB I get LD5 Red, LD7 Red and two user ...