Is it possible for stm32WB to recieve audio from a mobile device via bluetooth and at the same time send the audio to another device like headphones or wilreless earphones via bluetooth .Reception and Transmission should work simulteneously.Does it s...
I am using SAI protocol to get the audio output...For now I am directly using the bin file provided in the sample code...I just wanted to know if we have mp3 file or any other format other then bin file, how it can be dumped to board using STM32CubeP...
We figure that the STM32WB55 support only sending audio data through opus codec and doesn't have an A2DP behavior like other traditional BL. Could integrate an audio profile to the STM32WB for MP3, AAC, WAV
So I am trying to synchronize microphones with a clap board; that works nicely as-is but when I tried to change the N_MS_PER_INTERRUPT to 10 (on both BVOPUS_PER and BVOPUS_CEN), I get clicks in my audio signal.I've changedN_MS_PER_INTERRUPTAUDIO_OUT_...
Hi, I'm testing the STM32CubeFunctionPack_BVLINKWB1_V1.1.0 package. is it possible to stream audio from one device acting as central to more than one peripheral?