User Activity

So I am trying to synchronize microphones with a clap board; that works nicely as-is but when I tried to change the N_MS_PER_INTERRUPT to 10 (on both BVOPUS_PER and BVOPUS_CEN), I get clicks in my audio signal.I've changedN_MS_PER_INTERRUPTAUDIO_OUT_...
I have an existing phone app (using the traditional GATT system), and I would like mesh-enable my products so that if the products can see each other, then the phone can connect to and control any node (so, not so much an automation system but a rela...
How "reliable" should the connection be to PunchOut's LightBlue app?With -86dBm, I can connect to it ~40% of the time (other times it returns "no data" and goes back to the scanning screen)... below -93 dBm, I can see it, but I can't connect at all.A...
Is there a guidance sheet for the BlueNRG_Stack_Initialization_t structure passed into BlueNRG_Stack_Initialization?I've been using the SensorDemo application as a template, and found that I need to say#define MAX_NUMBER_ATTRIBUTE_SERVICE1 (13)Even t...
I wrote a version with 16 bit UUIDs, but it seems that LightBlue doesn't handle duplicate UUIDs in the same service (Service: Automation I/O; I added 4 analogs and 3 digitals; some are R/O and some are R/W, but LightBlue only is using the permissions...
Kudos from