STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1409 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 556 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! Unable to access the ST marketplace

Hello, my CubeIDE stuck while looping trying to access  the marketplace where I need to download and install EGit plugin. During this "looping" the window cannot cancel the operation , neither close the window - typical of Java' "runaway" ... After  ...

eBirdman by Senior II
  • 2007 Views
  • 6 replies
  • 0 kudos

Resolved! Deleting of ".elf" file in MacOS sequoia 15.2

 Hi everyone, I’m using a MacBook with an Apple M1 chip running macOS Sequoia 15.2. I recently updated STM32CubeIDE to version 1.18.1. My target board is a Nucleo-32 STM32L031K6T6. Initially, I created a new project using STM32CubeIDE and, without mo...

Tunahan by Associate
  • 1969 Views
  • 5 replies
  • 1 kudos

Resolved! Using Kiel for STM32F446 - trying to avoid CUBE

Hello,I have the very excellent book "STM32 Arm Programming for Embedded Systems" by Mazidi, Chen, Ghaemi.  It is from 2017.  The book uses Keil, which I am very happy to use, and it has very nicely written code which I fully understand (so nicely wr...

pdd_1234 by Associate II
  • 2709 Views
  • 7 replies
  • 1 kudos

Resolved! Error in build about MX_Init gpio and icache

Hello!When I build my project, I get these errors. I should note that the header files are in the driver folder, and I have added all the necessary include paths."C:/Users/helat/STM32CubeIDE/workspace_1.18.1/PFA-SecureM/Core/Src/main.c:90:(.text.main...

hela by Associate
  • 1155 Views
  • 2 replies
  • 0 kudos

How to compile OpenBootLoader code?

I am going to implement a boot loader code for stm32g431xx series chip. But I met a problem of compiling C files in the "OpenBootLoader" folder.  A lot of macro undeclared messages came out. Is there any suggestion to use the OpenBootLoader?   

Resolved! Main.c Not Generating

Hi I am new to STM32CubeIDE. I am setting up a blue pill board. I don't seem to have any issues with pin configurations however when I try to generate code I only get a refreshed .ioc file with only .project and .ioc in my project folder. Is there so...

Charlton by Associate
  • 1670 Views
  • 2 replies
  • 2 kudos