cancel
Showing results for 
Search instead for 
Did you mean: 

Using Kiel for STM32F446 - trying to avoid CUBE

pdd_1234
Associate II

Hello,

I have the very excellent book "STM32 Arm Programming for Embedded Systems" by Mazidi, Chen, Ghaemi.  It is from 2017.  The book uses Keil, which I am very happy to use, and it has very nicely written code which I fully understand (so nicely written!).

I am having trouble getting a project going in Keil because in the book when you make selections in 'Manage Run-Time Environment' during the project set up is says to tick 'System Startup for STMicroelectronics STM32F4 Series', but in my version of Kiel, it says something like 'use Cube IDE/MX' and no option to use 'System Startup for STMicroelectronics STM32F4 Series'.

Could someone help with this? I do NOT want to use Cube IDE etc. all that software its horrible.

Thank you in advance!

1 ACCEPTED SOLUTION

Accepted Solutions
pdd_1234
Associate II

The correct solution for this issue is to rollback the version of Keil/MDK to the version which does not integrate Cube MX automatically and instead uses the "start up" option.

This way you can avoid Cube MX and just use a simple #include stmxxxx.h and use clean, simple, bare metal code (albeit with CMSIS).

View solution in original post

7 REPLIES 7
mbarg.1
Lead

Why do you not ask Keil? I suppose you paid for that ...

No, I'm just studying. 

Probably you have to study a little more or better before asserting some code is horrible ...

There are many people that confuse something horrible with something beyond their intellectual capability ..

TDK
Super User

Why is it horrible?

If you feel a post has answered your question, please click "Accept as Solution".
ahsrabrifat
Senior II

You can get CMSIS and Startup Files from ST's GitHub

I presume you have looked at STM32 Arm Programming for Embedded Systems" by Mazidi, Chen, Ghaemi, but you like HAL and LL and your editor peppered with pre-written stuff you don't want, and that is why you're saying what you're saying. You also like cOde GenERatIOn.  That's why you're all salty

 

 

pdd_1234
Associate II

The correct solution for this issue is to rollback the version of Keil/MDK to the version which does not integrate Cube MX automatically and instead uses the "start up" option.

This way you can avoid Cube MX and just use a simple #include stmxxxx.h and use clean, simple, bare metal code (albeit with CMSIS).