STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1471 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 571 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

issue in opening two file in fatfs stmcube

Hello,I have been trying to open two files simultaneously in sdcard (one in READ mode and another one in Write mode) using the STMCUBE IDE fatfs library. Since two files requires two file handles so I have defined below mentioned parameters in the fa...

shefu_0-1715236162842.png
shefu by Associate II
  • 2964 Views
  • 4 replies
  • 0 kudos

Deprecated behavior of the linker

Hello ST community, I have cloned a project developed by a colleague of mine using STM32WBA52 MCU.When I hit build for the project I got this error "Note: This behavior is deprecated and will be removed in future version of the linker"I updated STM32...

Resolved! STM32CubeIDE typo error in debug mode window.

There is a typo error in debug mode window. While debugging, in the bottom right corner, the phrase "Description: Cortex-M4 core descriptions, generated from ARM develloper studio" contains a typo where "developer" is mistakenly written as "devellope...

STM32CubeIDE Typo.jpg
EDokm by Associate III
  • 692 Views
  • 1 replies
  • 0 kudos

Resolved! CubeIDE 1.18.1 generates wrong code for TIM15

We're using STM32CubeIDE 1.18.1 under Windows.  When generating LL_ code for a STM32C092, TIM15 init generates this code:static void MX_TIM15_Init(void) { LL_TIM_InitTypeDef TIM_InitStruct = {0}; /* Peripheral clock enable */ LL_APB2_GRP1_Ena...

Resolved! Error: failed to erase memory

Hi,While flashing code in STM32G474VBT6, I am getting below error. After reinstalling cube ide and cube programmer, same error continues. STMicroelectronics ST-LINK GDB server. Version 7.4.0Copyright (c) 2023, STMicroelectronics. All rights reserved....

Nsg1987_0-1691554608910.png
Nsg1987 by Senior
  • 34868 Views
  • 23 replies
  • 13 kudos

File folder not being included in build

I have been able to load the demo source code for the STM32F469I_Discovery from GitHub and get it to run as expected under TouchGFX. However, when I try to build it in STM32CubeIDE, the folder for the BSP is not included and the corresponding obj fil...

AndrewNeil_0-1750080456536.jpeg
DavePfz by Associate III
  • 1055 Views
  • 3 replies
  • 0 kudos