STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1406 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 556 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

STM32H757 dual core debugging issue

The last couple of months I have been developing on an STM32H757I-EVAL board. Programming and debugging (multi-core) works reasonably well; although sometimes I need to re-power the board.During the last weeks, we transitioned from the EVAL board to ...

MiNe by Associate
  • 672 Views
  • 2 replies
  • 0 kudos

Can't break at Cortex®-M4 address on STM32H7 dual core.

Hi All,I am using STM32H747IDISCO kit.I load example project HSEM_COreSync into STM32CubeIDE(version 1.18.1) , and set a breakpoint at"BSP_LED_On(LED3);" line in main function on Cortex®-M4 side. And I start debug, but break doesn't occur.I recognize...

Paco by Associate III
  • 921 Views
  • 2 replies
  • 0 kudos

Resolved! Issue with Starting Flashed Program at startup.

Hello,Excuse me for being such a noob here but I'm having an issue with an STM32H7A3RTI6. I flash a basic blinky program with the stlink and then when I go to disconnect/reconnect the stlink to supply power to the chip it doesn't start up the program...

Compilation Error when Using STM Cube IDE V 1.18.1

Hi, Error compiling. Error code isC:/ST/STM32CubeIDE_1.18.1/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.13.3.rel1.win32_1.0.0.202411081344/tools/bin/../lib/gcc/arm-none-eabi/13.3.1/../../../../arm-none-eabi/bin/ld....

choi04 by Associate
  • 786 Views
  • 1 replies
  • 0 kudos

STM32CubeIDE Zip File Reuired for Installation.

Heyyyyyyyyy St community. I need Help regarding the installation of STM32CubeIDE. I have been trying to Download the latest installer file from ST website but I am unable to download it. I changed my browsers, my PC, I even tired Downloading the file...

ZoyLeoz by Associate
  • 582 Views
  • 3 replies
  • 0 kudos

Resolved! Pin Configuration Panel Missing Drop-downs

I recently installed STM32CubeIDE on a new computer for the first time. Starting out my first project, and I immediately run into an issue that makes the MX portion basically completely un-usable. The problem is that when I want to change the configu...

image_2025-06-29_224319138.png

Resolved! Signal Handler Called at 0xFFFFFFF9

My code gets complied without any errors. But just before the uploading completes: <signal handler> called at 0xfffffff9 is displayed.Even though after that my code runs properly without any hardfault.

Resolved! How to change the STM32 family in a project using HAL?

Hello,I am currently using a F4 processor in HAL together with the Stm32cubeIDE.Thus the IDE generates F4 hal files which later are included in the main program.  To access the specific functions I need to #include "stm32f4xx_hal.h" in my own program...

DocAlex by Associate III
  • 1598 Views
  • 5 replies
  • 2 kudos