STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1410 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 557 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

STM32CubeIDE - how to program my device permanently?

Hi there,I have been using STM32CubeIDE for a few days now and really like it. I have managed to run some code and successfully debug my code using ST-LINK and the embedded debugger of STM32CubeIDE.I now would like to program my device so that the co...

Roberto.F by Associate II
  • 2402 Views
  • 5 replies
  • 0 kudos

How to set SYSCLOCK to 400 MHz using STM32CubeIDE?

I am using a NUCLEO-H743ZI board. Using STM32CubeMX, I was able to set SYSCLOCK to 400 MHz like so:With STM32CubeIDE, it won't allow me to do the same:What should I be doing here instead?STM32CubeIDE has been really frustrating.

0690X000008wCwEQAU.jpg 0690X000008wCwOQAU.jpg
edwin8 by Associate II
  • 2096 Views
  • 3 replies
  • 0 kudos

STM32F303K8 - CAN bus doing nothing?

Hi there,we are using the STM32F303K8 with the NUCLEO-F303K8 board. I installed the latest STM32 Cube IDE v.1.0.0 and wanted to get the CAN bus working.So after searching for the latest documentation it took a while to figure out the new can bus impl...

MP.17 by Associate II
  • 1674 Views
  • 1 replies
  • 0 kudos

Is it possible to enable SWV for STM32F030?

I just installed STM32CubeIDE 1.0 version to give it a try. When I tried to enable SWV , i saw it is disabled and can not modifiable. At first, I assumed this is because of some limitation of chip, but with same hardware my other compiler ( Keil ) i...

KG?�l by Associate II
  • 2639 Views
  • 4 replies
  • 0 kudos

STM32F103ZET error: No device found on target.

After I click DEBUG ,it shows that Error in initializing ST-LINK device.Reason: No device found on target.I think it's not hardware's problem because I can download my program in Keil uvision successfully. and my debug configuration is showed as foll...

0690X000008BZDuQAO.png 0690X000008BZDzQAO.png
RRuan by Associate II
  • 3888 Views
  • 9 replies
  • 0 kudos