STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1244 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 511 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

HAL_Delay does not work

I built my first board with a STM32F030CC mcu. I downloaded STM32CubeIDE and created a new project. I set PA8 as a GPIO output port.All I want to achive is to enable/disable the LED connected to the PA8 port .My problem is, that HAL_Delay does not wo...

PMind by Associate II
  • 3523 Views
  • 5 replies
  • 0 kudos

Resolved! Software download issues

When i "click on this button to validate your email address and start the download of the requested software" there is no links to dowload IDE.

VBelo by Associate
  • 1018 Views
  • 1 replies
  • 0 kudos

Why would a default project generated with NO modifications (stm32767ZI eval board) fall into a configASSERT inside xQueueSemaphoreTake()?

The line is in queue.c : configASSERT( !( ( xTaskGetSchedulerState() == taskSCHEDULER_SUSPENDED ) && ( xTicksToWait != 0 ) ) );I selected in th device config: USB_HOST, LWIP, FREERTOS, FATFS, USART1,USART3, USART6, UART7, UART8, ETH and TIM1 for use ...

FBrow by Associate II
  • 801 Views
  • 0 replies
  • 1 kudos

STM32CubeIDE randomly closing

If I leave it alone for at least a few hours it seems to decide to close itself. I haven't worked out that it's any sensible time so possibly a memory leak ?

MikeDB by Lead
  • 757 Views
  • 0 replies
  • 0 kudos

Bug with single wire UART

Hey there,it's no big deal, but rather annoying. If I select one UART to be Half-Duplex the RX pin disappears from the pinout even if I select receive only. It doen't matter if I select RX only or TX only, the RX-pin won't show up again. The generate...

EKoec by Associate II
  • 1084 Views
  • 0 replies
  • 0 kudos