cancel
Showing results for 
Search instead for 
Did you mean: 

Bug with single wire UART

EKoec
Associate II

Hey there,

it's no big deal, but rather annoying. If I select one UART to be Half-Duplex the RX pin disappears from the pinout even if I select receive only. It doen't matter if I select RX only or TX only, the RX-pin won't show up again. The generated code also initializes only the TX pin. Boooo.

I'm using STM32CubeIDE

Version: 1.0.0

Build: 2872_20190423-2022 (UTC)

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0