STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1245 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 511 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Change static library project target device in STM32CubeIDE

I'm creating a static library project that is portable across many mcu because it is target indipendent code. The problem is that once I created the project, it seems impossible to change che mcu setting inside Project Properties > C/C++ Build > Sett...

0690X000008ivW8QAI.png
RMais by Associate II
  • 941 Views
  • 0 replies
  • 2 kudos

STMCubeIDE Defaults

In the new project setup, the default minimum heap and minimum stack size are set to 0x200 and 0x400, but despite being in black they seem to be non-editable. For a large processor these numbers are far too small, especially the stack.And yes I kno...

MikeDB by Lead
  • 1664 Views
  • 3 replies
  • 0 kudos

Resolved! Clock Configuration with STM32CubeIDE

I am new ti STM32CubeIDEI am trying to use the visual clock configuration tool.What I can't figure out is how do I select HSE in the PLL Source Mux? It seems to be disabled in the tool.

0690X000008itKoQAI.png
KMill by Senior II
  • 3943 Views
  • 2 replies
  • 0 kudos

STM32CubeIDE and Segger JLink cannot be simultaneously installed! (conflicts with Segger JLink due to udev rules conflict)

If Segger JLink is installed, STM32CubeIDE cannot be installed. See here: https://community.st.com/s/question/0D50X0000AmhtsLSQQ/stmcubeide-installer-failed-on-ubuntu-1804-with-a-dependency-errorIf STM32CubeIDE is installed, Segger JLink cannot be in...

GStap by Associate II
  • 2507 Views
  • 2 replies
  • 0 kudos

Resolved! MacOS Install queries

Installing the latest STM32CubeIDE on mac is problematic.I am running MacOS 10.14.5 (Mojave)The install for ST-LINK Server fails with an error about it being incompatible and harmful.If I selected "New STM32 Project" then the following dialog appears...

0690X000008ifQEQAY.png 0690X000008ifRCQAY.png 0690X000008ifQ4QAI.png
KMill by Senior II
  • 1578 Views
  • 2 replies
  • 0 kudos