STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1249 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 512 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

How do I report a critical bug to ST?

There seems to be a bug that causes you to lose your files. I'm running version 1.0.1 of CubeIDE (build 3139_20190612-1256). When I tried to create a new project in my C:\Projects folder, I thought the IDE would create a new folder inside C:\Projec...

ministm32f103rbt6 hardware.

i am using ministm32f103rbt6 hardware. in stm32cubeide it is showing nuleo to geenrate a project. which board should i select .  please guide me for this controller to work on stm32cubeide. for can communication program how to configure. i am new to ...

Kpras by Associate
  • 977 Views
  • 1 replies
  • 0 kudos

Flash memory & SD Card

Hello everyone, just I want to know a little detail: when I’m debugging my program (C file) I suppose it goes to the flash memory! I want to know if it’s possible to debug to SD Card?

idrissmc by Associate III
  • 1466 Views
  • 3 replies
  • 0 kudos

Follow others custom usb hid demo but not work.

I first used a stm32f103 board,after generated code and configurated usbd_custom_hid_if.c and then download the code,my computer cant recognize the usb device.Then I changed to a f407 board, after done the same work,my computer can recognize the devi...

Mcfly by Associate
  • 798 Views
  • 0 replies
  • 0 kudos

Repeatition counter problem in STM32G431RB DISCO + CubeIDE

Hello.There are some problems with the repeatition counter (TIMX_RCR).The problem occurs when I enable the OPM setting to use the feature and enter a 16 bit value in the RepetitionCounter setting.I think that it is correct to change uint8_t Repetitio...

MKim.5 by Associate
  • 1774 Views
  • 3 replies
  • 0 kudos

How to use GCov in STM32Cube IDE and STM32F4

Hello,I have tried to set up GCov in STM32Cube IDE using this tuto:https://mcuoneclipse.com/2014/12/26/code-coverage-for-embedded-target-with-eclipse-gcc-and-gcov/I am using a STM32F413 and when I compile I got an overflow on RAM section by 150Kbytes...

ABern by Associate II
  • 2502 Views
  • 0 replies
  • 4 kudos

printf float STM32G070CB

How to enable float (printf) in STM32CUBEIDE 1.0.1 IDE?The -u printf_float option is selected.

RDos by Associate II
  • 1460 Views
  • 2 replies
  • 0 kudos