STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1262 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 512 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Nucleo-H743zi standard output to the STM32CubeIDE console

I have a Nucleo-H743zi board and am debugging an application using STM32CubeIDE. There is some legacy code that does some debug printf's I don't see anything on the debug console or the regular console. How does one configure standard output to r...

MRait.7 by Associate
  • 2008 Views
  • 4 replies
  • 0 kudos

Getting Started with STM32H750B-DK

I want to start writing my own code for the STM32H750 discovery board. I have installed STM32Cube IDE, MX and PROG. I have downloaded the examples for the board and I'm trying to build and run the GPIO example because its the simplest. I've chosen th...

IGeor by Associate II
  • 1304 Views
  • 0 replies
  • 0 kudos

Generating code removes my added include paths

Hi, It's my first time using STM micros and the Cube IDE.Whenever I generate code from the device configuration tool, the include paths I have added in properties > C/C++ Build > Settings > MCU GCC Compiler > Include pathsdisappear. This only happens...

JKape by Associate
  • 813 Views
  • 0 replies
  • 1 kudos

STM32F030 Erase internal flash page

Dear,I made a project for STM32F030RC with STM32CubeIDE. when I use "HAL_FLASHEx_Erase" function to erase some flash pages (at end of flash that there is no code on it) , the CPU crash. I guessed it is depended on interrupts. so I disabled interrupts...

Load symbols from more than one elf file

I have a bootloader + main application that I would like to debug. Unfortunately it looks like I can only specify 1 file to load the symbols from? In TrueStudio it was easy with the debug script file to specify more than one, but the simplified UI ...

LKory by Associate
  • 2124 Views
  • 2 replies
  • 0 kudos

Getting started with STM32CubeIDE questions

Question 1: I just installed STM32CubeIDE on my home computer and my work computer. When I start a new project for the STM32L4R9I-Disco discover kit on my home computer the CubeMX tool opens fine with no initial errors or warnings on pins. When I s...

magene by Senior II
  • 1444 Views
  • 2 replies
  • 0 kudos

Problem with adding a Library to the Projekt.

I can add the Library over the Properties of Project. Under the c/C++ General topic, Paths and Symbols. With the Tab Libraries.There i can Add it with the Button Files System. But if i Build it, i get following Error Message.How can i solve it? cann...

kcrh73 by Associate
  • 764 Views
  • 0 replies
  • 0 kudos