STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1259 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 512 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! printf() not working - _write() never gets called

Hello,as the title suggest, I can't get printf() to work.I implemented _write() in my main() but during debugging the program never get there.The project was created with CubeIDE.int _write(int file, char *data, int len) { if ((file != STDOUT_FILE...

CKauf by Associate III
  • 15850 Views
  • 9 replies
  • 3 kudos

CubeIDE not updating Debug Configurations

I am trying to switch from eclipse to CubeIDE. But it wont let me save the debug configurations. I have imported the project, build it, when trying to debug it doesnt let me press(Debug As AC6 Application) When trying to add my own debug configuratio...

RDe V by Associate
  • 1358 Views
  • 1 replies
  • 0 kudos

Resolved! How to install an Eclipse CDT Plugin like OpenMRC?

Dear Friends, I'm having problems to load this plugin (Eclipse CDT Plugin: OpenMRC), it's from GitHub, I tried using the "Install New Software" but without good results, I also download it to my desktop but the IDE wants JAR files, so please someone ...

0690X00000A9k26QAB.jpg
HLare by Associate
  • 2194 Views
  • 2 replies
  • 0 kudos

Where is the C++ support in STM32CubeIDE?

When starting a new project in STM Cube IDE there is an option given to generate C++ instead of C code but when selected I still get the same generated c code... If I wan't to use modern C++ conventions what are my options or should I be looking at a...

norlesh by Associate III
  • 2123 Views
  • 3 replies
  • 1 kudos

Resolved! STM32CubeIDE library inclusion error !!!

I downloaded the X-NUCLEO-IHM01A1 from the st website and loaded an example project in stm32cubeIDE, however I keep on getting the library inclusion error.

0690X000009YpmRQAS.png
Cash by Associate II
  • 1476 Views
  • 1 replies
  • 0 kudos

Device Configuration Tool Resets Project Properties.

Hi,I upgraded to the latest version of STM32CubeIDE (Version: 1.0.2) and I am noticing a possible bug with the device configuration tool. Whenever I open the tool and generate code from it, it resets all my build and general properties. This is reall...

PShut by Associate
  • 902 Views
  • 0 replies
  • 1 kudos