STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1426 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 558 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

How import mbed project on stm32 cubeide?

Hello everyone, this is my firt question, sorry for my error. I have create a little program on mbed online compiler, but now i would import this program on stm32cubeide for use debug. Online i have see some tutorial but they are old and don't work. ...

Why don't user debug scripts work with STM32CubeIDE ?

When I specify a user debug script in STM32CubeIDE debug configuration window I get the error "Provided file doesn't exist" even though it's there. Even if I specify the same text as the "Automated Generation" option I get this error.Is there a worka...

0690X000009YeY2QAK.jpg
dave2012 by Associate III
  • 2657 Views
  • 10 replies
  • 0 kudos

STM32CubeIDE 1.1.0 LL GPIO bug? (stm32g0xx_ll_gpio.h)

Shouldn't these be (Pin * 2U) , or (Pin + Pin)?__STATIC_INLINE void LL_GPIO_SetPinMode(GPIO_TypeDef *GPIOx, uint32_t Pin, uint32_t Mode) { MODIFY_REG(GPIOx->MODER, ((Pin * Pin) * GPIO_MODER_MODE0), ((Pin * Pin) * Mode)); }   __STATIC_INLINE uint32_...

BCoch by Senior
  • 1203 Views
  • 1 replies
  • 0 kudos

Resolved! Undefined referenece to error

Hi,from Properties -> Paths and Symbols i added file path to 'Include Directories'. Then, i added my source file and my header file to 'my_libs' which i created under project_name -> Drivers.When i call a function from library i see 'undefined refere...

STM32F303CCT6 OpAmp in STANDALONE mode, gain very low.

Hi all!, I have a electret microphone amplifier (see attached). The circuit works fine with a LM-358, but when I use the internal opamp from a STM32F303, the gain is very low. I use the STM32 opamp in STANDALONE mode. Is ther something I'm missing?I ...

JAlca by Senior
  • 1324 Views
  • 0 replies
  • 0 kudos

How to set tool paths?

I attended a recent ST seminar and was delighted to see the improvements in STM32CUBEIDE! Worked great in the seminar and I completed all 6 projects using MEMS components.It's now been about a month and I'm wanting to spend some serious time with the...

doctek by Associate II
  • 1368 Views
  • 1 replies
  • 0 kudos