STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1418 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 558 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Problem Nucleo-L152RE USB CDC

I use the STm32CubeIDE and want to use the CDC USB Port on a Nucleo-152RE Board. I have configured all things in the Cube and the code is generated. But when I plug in the USB in the pc, no com-port will appear. What do I wrong?Thanks for your help.

s.berl by Associate
  • 783 Views
  • 0 replies
  • 0 kudos

Setup FreeRTOS and USB Host with STM32CubeIDE

I'm new to STM32 so I am learning FreeRTOS using this video https://www.youtube.com/watch?v=OPrcpbKNSjU&list=PLEBQazB0HUySNug4eRm-73hNyMcCRViRB&index=3 but with the STM32 F4 Discovery board, so the STM32CubeIDE (v1.1.0) has both FreeRTOS and USB_Host...

MartinC by Associate
  • 4796 Views
  • 1 replies
  • 2 kudos

Problem with FreeRTOS on STM32F103RB

Hi,Recently I tried to install FreeRTOS on my STM32F103RB and when I finished the installation and configuration I got a compilation error. I need a solution to this problem.The problem looks like this:13:57:07 **** Incremental Build of configuration...

How do I import TrueStudio project for BlueNRG-2?

The BlueNRG-1/2 SDK provides sample projects in TrueStudio form. When I attempt to import any of them into STM32 CubeIDE, I am presented with a dialog asking for the proper MCU for the evaluation board. If there is a way to determine the correct an...

0690X00000Arj6KQAR.png
BBeau by Associate
  • 1472 Views
  • 1 replies
  • 0 kudos

STM32CubeMX file => linker script file not generated properly

Hi,I'm using STM32CubeIDE with a former Atollic TrueStudio project. The import itself succeeded, but it's neccessary to fine tune the settings. Also, when using the STM32CubeMX files, it seems that STM32CubeIDE uses different file names for several s...

RAltm by Senior
  • 4005 Views
  • 7 replies
  • 0 kudos