cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeIde resets include paths when build hardware project

FedeRico1
Associate II

Hi there,

I'm using STM32Cube Ide to work wih my STM32F7.

I really like this software also for the integration of STM32CubeMX.

I use the STM32CubeIde to configure the hardware, peripheral, OS and so on but when I build the configuration I noticed that also the Include Path are restore.

So every time I change a perpheral setting and I rebuild the the project, the project lost the setting and I need to add manually every source folder that I added.

Is there a way to avoid this?

Thanks for the help.

BR,

Federico

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
Cartu38 OpenDev
Lead III

Definitively a bug.

Sounds some improvements have been done Thanks STM32CubeIDE V1.1.0 just released on st.com

JKlyn.1108
Associate

For me, 1.1.0 has problems on MacOS. I cannot get ST-Link debug to work, only OpenOCD. 1.0.2 works fine (except the bug above, very annoying!) These tools are rather disappointing.

Cartu38 OpenDev
Lead III

"1.1.0 has problems on MacOS" what do you mean ? Is such still related to "resets include paths when build hardware project" i.e. your post header or MacOS issues in general relying on 1.1.0. If general 1.1.0 MacOS issue I obviously agree according numerous post about.

JKlyn.1108
Associate

I have the same problem as OP, and in addition, on MacOS, the ST Link debugging doesn't work. It does work on 1.0.2