STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1433 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 560 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Updated HAL documentation for CAN driver in STM32F1 ?

I want use the CAN on a STM32F103.I note some difference between HAL documentation I have, and the HAL driver.The documentation is UM1850 rev 20 (april 2017).I don't know the version of the HAL driver, it's in STM32CubeIDE 1.0.2for example, in docume...

jihzed by Associate II
  • 1027 Views
  • 0 replies
  • 0 kudos

QSPI with stm32cubeIDE on custom stm32f746IGT board

Is there any one to help me on get QSPI work?I am using n25q128 and the SPI pins; /**QUADSPI GPIO Configuration      PE2    ------> QUADSPI_BK1_IO2   PF9    ------> QUADSPI_BK1_IO1   PB2    ------> QUADSPI_CLK   PD11    ------> QUADSPI_BK1_IO0   PD13...

istepne by Associate III
  • 6882 Views
  • 19 replies
  • 0 kudos

STM32 NUCLEO-L053R8 + SDCard basic example

I'm quite new in STM32 applications. I'using a Nucleo-L053R8 and I need to store the data from ADC inputs in a SD card. I found some examples but with different MCUCan anyone help me sharing a basic and full working example developed in CubeIDE?.

Brugus by ST Employee
  • 1426 Views
  • 1 replies
  • 0 kudos

Error During creating new project in STCube v1.1.0

Goodevening,I'm new on this community and i I want to apologize in advance if I make some mistake. My problem is: when i create new STM32 project i get this error "Code generation could not be done because the necessary firmware package is missing. N...

There are a large number of existing STM32 sample projects set up to work with EWARM, MDK-ARM and SW4STM32. Even though use the migration guide for importing projects into STM32CubeIDE most of the time these projects do not import properly.

Are there any instructions on how to import an existing STM example project into STM32CubeIDE such that is can be built and deployed. At the moment its a very frustrating process that wastes lots of time and energy.

request: board examples using the CubeIDE project structure

When stumped, I've found that the examples in the various board zip files that STMCubeIDE downloads are very helpful. However none of them are structured in a way that I know how to load into the 'modern' STM32CubeIDE. is there any documentation aime...

mmalex by Associate II
  • 1229 Views
  • 1 replies
  • 0 kudos