cancel
Showing results for 
Search instead for 
Did you mean: 

v1.0.1 does not open MX configs from v1.0.0 anymore

pierpaolo
Associate II

As title.

When I open a .ioc MX configuration of a project with the newest version, the IDE hangs at "Initializing Device Configuration Tool".

This discussion is locked. Please start a new topic to ask your question.
8 REPLIES 8
Markus GIRDLAND
ST Employee

I just did a test on my Windows and I can't reproduce this.

What operating system are you using?

And just to make sure:

You're creating a project in 1.0.0 and then you open it in 1.0.1 and when you try to edit in the .ioc file you get stuck at "Initializing Device Configuration Tool", right?

pierpaolo
Associate II

That is right.

I'm using Mac.

The project is configured with USART1 and USB CDC (STM32WB55).

I was able to reproduce it when I used a mac computer instead.

I'll make a ticket for it, thanks for the feedback!

EKrum
Associate II

I am having this same issue as well, and I am using Mac OSX 10.14.5

EKrum
Associate II

I was able to open the MX file if I edited the .ioc file to bump the version numbers. I made the following changes:

MxCube.Version=5.2.0 ==> MxCube.Version=5.2.1

MxDb.Version=DB.5.0.21 ==> MxDb.Version=DB.5.0.21

However, I do not know if this introduces any new errors, so proceed with caution.

Bav
Associate

I have just installed this on a Mac to see if I wanted to move from SW4STM32. I installed V1.0.1 and made a test project. Then I was told that there was a version 1.0.2 so I installed that. Now it hangs trying to open the ioc as the OP describes.

RMart.525
Associate

Same issue with 1.1. Is anyone fixing bugs?

Ron Koch
Associate II

Same problem with MX version 5.4.0. How do I find out what the correct MxDb.Version should be set to? Is there anything else I need to do to convert an '.ioc' file?