STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1688 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 633 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

From TrueStudio to STM32CubeIDE how to?

Until now I used TrueStudio.But now I generated a project for STM32CubeIDE, suing the seprated CubeMX.I'm using STM32CubeIDE Version 1.3.0, STMCuneMX Version 5.6.1Reinstalled both, but no luck to get it working on Windows 10.And get these error when ...

Jack3 by Senior III
  • 1530 Views
  • 2 replies
  • 0 kudos

Resolved! Programming STM32 in bootloader mode under Linux

Good evening (o;Now that my test setup works fine with setting the RTC via USB CDC and entering USB DFU mode due to the excellent help from the community members here....the next little problem arises (o;Which program can be used nowadays under Linux...

Davorin by Senior
  • 11197 Views
  • 4 replies
  • 0 kudos

Binary output code

Hi all,I'm working on TouchGFX project that uses external QuadSPI Flash to store all graphics objects required by my designed HMI.I want to obtain as result of the release building two distinct .bin files that contain respectively: one bin file that ...

EBris.2 by Associate
  • 1643 Views
  • 2 replies
  • 0 kudos

Where to place own source/header files on CUBE IDE?

Even copying and pasting my *.h & *.c files into my new project CUBE IDE does not accept these files, issuing: "No such file or directory" and aborting the compilation. What should I do? My bult: Version: 1.3.1Build: 6291_20200406_0752 (UTC)

JSILV.2 by Senior
  • 1279 Views
  • 2 replies
  • 0 kudos

Hello, I get a problem debugging my program and I don't know how I can resolve it as my parameters seems good. I am using a NUCLEO32-L432KC with STM32CubeIDE.

My problem is that when I want to debug my firmware, i get a message saying " 'Launching <MyProgram> Debug' has encountered a problem. Failed to execute MI command : <C://____/MyProgram.binary: No such file or directory."That is true I have not a .bi...

Zephyr S by Associate II
  • 1699 Views
  • 2 replies
  • 0 kudos

Static Library for STM32H753

I am trying to generate a static library which calls FreeRTOS functions listed below -osThreadDef and osThreadCreateosSignalSet and osSignalWaitosDelayosMutexCreate etc.in System Workbench for STM32.Without including the FreeRTOS Utilit...

C local application program is not running properly in IDE's console however it runs properly on Code::Blocks IDE. Looking for assistance on this issue.

Running a very basic C program that prompts user for input from console, grabs input and then does computations and generates output on console.When I run my program as "Local C/C++ application", on console, it appears to be waiting for something su...

JH.1 by Associate
  • 1711 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE Copy project issues

Hello,I noticed that when I want to copy a project into the same workspace, the following issues occur:If the project to copy is the only one into the workspacace, when I paste it, the IDE pops-up a message for a "null argument" error...If there are ...

simo zz by Senior II
  • 2137 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.