STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1409 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 556 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Problems with downloading program.

Hello,if I try to download my program from STM32CubeIDE, the following will happen:STMicroelectronics ST-LINK GDB server. Version 5.2.3 Copyright (c) 2019, STMicroelectronics. All rights reserved.   Starting server with the following options: ...

0693W000001sheGQAQ.png 0693W000001sheLQAQ.png
Moritz1 by Associate III
  • 1488 Views
  • 4 replies
  • 0 kudos

Failed to start GDB server

,I have STM32F446 board. I am trying to debug a code, but it states that Failed to start the GDB server. I have attached a photo for the problem.Could anyone support to solve this issue.

0693W000001sjt3QAA.png
KIbra.1 by Associate
  • 1459 Views
  • 2 replies
  • 0 kudos

Resolved! STM32 DAC DMA Underrun problem

Hi, I am currently working on small project which I need to generate some arbitrary signal using DAC inside STM32G431KB.Code is shown below.#include "main.h" #include "SysClockConfig.h"     uint16_t Output_Buffer[10] = {2048,2048,2048,2048,2048,2048,...

LLOLO.1 by Associate II
  • 3373 Views
  • 3 replies
  • 1 kudos

Why USB CDC fails on open if cache is not enabled?

I have created a project with STM32cubeIDE using usb CDC. If cache is not enabled, accessing via firmware a specific variable located at ox20005604 (for example reading it) once a time, it causes that subsequent open from PC of the serial port retur...

AIach.1 by Associate II
  • 1285 Views
  • 2 replies
  • 0 kudos

I will try to ping another ip with STM32F207VG.

I pinged STM32 with my PC.However, STM32 did not find a way to ping another ip.Ask for advice.I am using STM32F207.I'm using STM32CubeIDE.I am using FreeRTOS.I called functions in api_lib.c to connect the network.The PC pinged STM32 and the response ...

Lyoun.1 by Associate
  • 778 Views
  • 0 replies
  • 0 kudos

Resolved! Debugging .hex file on STM32f469i Board

Hello All,I want to load AND debug a precompiled .hex file onto my STM32f469i Discovery board. I've looked around and tried several tools such as the STM32CubeIDE and the ST-Link utility, but no luck. The CubeIDE seems to be unable to flash the file,...

TLian.11 by Associate II
  • 5840 Views
  • 10 replies
  • 0 kudos