Skip to main content
MBaal
Associate
August 26, 2019
Question

Unhandled event loop exception

  • August 26, 2019
  • 3 replies
  • 2496 views

Hello,

with version STMCubeIDE 1.0.2, I get an 'unhandled event loop exception' after I've created a project and atttempt to look at the source code that is generated.

Effectively, this renders the IDE unusable, as the only option I have is to quit, as this errors keeps repeating itself.

It is hard to find out what is causing this bug, as the popup window is the only thing I can click in...

any ideas?

I'm using Ubuntu 18.04 to run this on and installed from the debian package for 1.0.2.

These errors started occuring after I updated from 16.04 to 18.04. But I reinstalled the STMCubeIDE...

This topic has been closed for replies.

3 replies

MBaal
MBaalAuthor
Associate
August 27, 2019

Some more detailed info when starting from the command line; the error messages are repeating numerous times, but I cut them here for brevity.

***WARNING: Detected: GTK_IM_MODULE=xim. This input method is unsupported and can cause graphical issues.
***WARNING: Unset GTK_IM_MODULE or set GTK_IM_MODULE=ibus if flicking is experienced. 
 
(STM32CubeIDE:9022): GLib-CRITICAL **: 14:01:52.225: g_base64_encode_step: assertion 'in != NULL' failed
 
 
 
(STM32CubeIDE:9022): Gtk-CRITICAL **: 14:02:25.858: gtk_box_gadget_distribute: assertion 'size >= 0' failed in GtkScrollbar
 
 
 
(STM32CubeIDE:9022): Gdk-CRITICAL **: 14:02:28.017: The window 0x7f75de488af0 already has a drawing context. You cannot call gdk_window_begin_draw_frame() without calling gdk_window_end_draw_frame() first.

MBaal
MBaalAuthor
Associate
August 27, 2019

Doing

export GTK_IM_MODULE="ibus"

before starting stmcubeide seems to fix it...

though a lot of the error messages still happen. (the encode step and the scrollbar one)

LAuda.1
Visitor II
June 21, 2020

I have been having the same Unhandled event loop exception problems. I'm running Debian 9, and getting rid of it, has been a real pain. Its related to the input ibus=xim bug

Here is a link talking about linux input handling . https://unix.stackexchange.com/questions/260601/understanding-setting-up-different-input-methods

Test with eclipse Version: 2020-06 (4.16.0) Build id: 20200615-1200 to see the problem.

It warns you about input , GTK_IM_MODULE="xim" being set, on startup (run from bash to see this startup warning)

you can use, im-config to change it, (install if you don't have ) to something else, but this dose not fix the problem!, X startup being complete abomination. It could being set in any number of other places. I removed ibus, nope, still get the warning from eclipse and the buffer flashing problem, and grep-ing all my config file's for gnome/gtk/X.. nop.. still could not find where it was being set, best I could come up with was to add this to .profile and .bash files

export GTK_IM_MODULE="gtk-im-context-simple"

export QT_IM_MODULE="simple"

This fix the problem for the moment(for me) but who knows, given the Java/Eclipse version nightmare, it may all stop working just by clicking the left mouse button at the same time your holding the Num lock key down, format your hard-disk, sign you up for a million $ loan at 200% interest , with your local shark loan organization, and then say.. Have a nice day!

Lachlan

LAuda.1
Visitor II
June 21, 2020

Not quite there, fixed the flashing window problem but not the crash Unhandled event loop exception

so change my version of have Java to oracle.com 1.8.0_251 . (version) Note ST ships it's own version of java, which apear's to be openjdk version "1.8.0_242"

as STMCubeIDE looks for it's own version not the system version you will have ln -s to the new version of java, ST version is at /opt/st/stm32cubeide_1.3.0/jre/

for now it's working.. touch wood(my head!) LOL

Lachlan