Skip to main content
PGroe.2
Associate III
June 16, 2020
Solved

Enable automatic code generation STM32CubeIDE

Hi,

I work with STM32CubeIDE

Version: 1.3.1

Build: 6291_20200406_0752 (UTC)

I somehow managed to disable automatic code generation for altered *.ioc file.

Now it doesn't automatically regenerate the source files according to the changes

I made in the configuration window for my STM32... instead it just shows a bracketed text

besides my *.ioc file in the Project Explorer so I have to click on the "Device Configuration Tool Code Gerneration" button to generate it.

If I remember correctly there was once a question if I want to auto-generate the code.

It seems I denied the question and ticked the "do not ask again" field. How can I revoke that decision?

This topic has been closed for replies.
Cartu38 OpenDev
Cartu38 OpenDevBest answer
Graduate II
June 19, 2020

You can revoke your decision relying on Windows>Preferences>STM32Cube>Device Configuration Tool.

​

By the way asking for code generation if .ioc editor active if possible either relying on Project>Generate code or pushing gear wheel in the toolbar.​

1 reply

Cartu38 OpenDev
Cartu38 OpenDevBest answer
Graduate II
June 19, 2020

You can revoke your decision relying on Windows>Preferences>STM32Cube>Device Configuration Tool.

​

By the way asking for code generation if .ioc editor active if possible either relying on Project>Generate code or pushing gear wheel in the toolbar.​