STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1409 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 557 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! Stm32CubeIDE | Most reliable version

Hi everyone, I'e been working with a fw stm32 MCUs products in the last years and I want to decide which is the best way to proceed in the "update to latest version" of CubeIDE.The point is: once i start a project, I usually keep the same CubeIDE ver...

Zzaaack by Associate III
  • 1043 Views
  • 1 replies
  • 0 kudos

About the Hierarchical of ST-Project on STCubeIDE

Hi, Recently, im go into some AI-integrated project. With the repos ST-model-zoo-service. Im wondering about these structural template. About how to import these template(like can i create a template like that, for both nested-project and structural ...

complete STM32CubeIDE Basics course on MacBook Pro?

I have Windows 11 running on Parallels and can't get ST-Link working. Will I be able to complete the STM32CubeIDE Basics course on a MacBook Pro (MacOS) with Apple silicon? I'm asking because the course prerequisites specifically call for a Windows P...

DanG_54 by Associate
  • 568 Views
  • 1 replies
  • 0 kudos

"Connection to MyST" Does Nothing

When I try to log into myST from the IDE, it literally does nothing. I click on the button, but no window pops up, nothing happens in the browser, nothing happens in the IDE, no new windows are created. I don't even get any output on the CLI (if I st...

antonly_0-1754908046465.png
antonly by Associate
  • 614 Views
  • 2 replies
  • 0 kudos

Resolved! live expressions bug

I use STM32CubeIDE version 1.14.1. When I'm in debug mode, the Values in the "Live Expressions" window are weird and wrong.However, I found out that after editing and putting a random value in one of the fields, it will be fixed.Beginning:  After wri...

beginning.png after edit.png

Resolved! not all register bits of nucleo-F439ZI are shown

Hi! I wish you are doing great!My problem is, I'm working on nucleo-f439zi board, in the reference manual, in register Flash-OPTCR, bit 4 is BFB2.But, when I choose the correct board (Nucleo-F439ZI), and go to debug mode, then SFRs, I only find F429 ...

0693W00000WJgWKQA1.png
OMuha.1 by Associate
  • 1167 Views
  • 2 replies
  • 0 kudos

Stm32f401ret6 with BNRG2A1

Dear TeamI am currently working on a BLE Mesh implementation. I have added the libraries in the project settings, but I am still getting errors. Please kindly respond.Description Resource Path Location Typecannot find -llibBlueNRG_Mesh_CM4-BNRG2A1_wc...

Kumar123 by Associate III
  • 827 Views
  • 3 replies
  • 0 kudos